Logo
Developing with ZBOSS for Zigbee
zb_zcl_device_management_set_event_cfg_payload_s::zb_zcl_device_management_set_event_cfg_by_list_payload_s Struct Reference

#include <zb_zcl_device_management.h>

Data Fields

zb_uint8_t event_num
 
zb_uint16_tevent_id
 

Detailed Description

Event Configuration Payload Format if Configuration Control field value is set to Apply by List.

Field Documentation

§ event_id

zb_uint16_t* zb_zcl_device_management_set_event_cfg_payload_s::zb_zcl_device_management_set_event_cfg_by_list_payload_s::event_id

The Event ID field represents the attribute ID of the event configuration attribute.

§ event_num

zb_uint8_t zb_zcl_device_management_set_event_cfg_payload_s::zb_zcl_device_management_set_event_cfg_by_list_payload_s::event_num

The Number of Events field represents the number of events contained within the command.


The documentation for this struct was generated from the following file: