#include <zb_zcl_device_management.h>
Data Fields | |
| zb_uint8_t | log_id |
Event Configuration Payload Format if Configuration Control field value is set to Apply by Log type.
| zb_uint8_t zb_zcl_device_management_set_event_cfg_payload_s::zb_zcl_device_management_set_event_cfg_by_log_type_payload_s::log_id |
The Log ID field represents the log ID of events to be updated with the new Configuration Value field passed in the command.