Logo
Developing with ZBOSS for Zigbee
zb_zcl_device_management_report_event_cfg_payload_s Struct Reference

ReportEventConfiguration Payload Format More...

#include <zb_zcl_device_management.h>

Data Fields

zb_uint16_t event_id
 
zb_zcl_device_management_event_cfg_attr_t event_cfg
 

Detailed Description

ReportEventConfiguration Payload Format

See also
SE spec, Figure D-157
zb_zcl_device_management_report_event_cfg_cmd_payload_t::event_cfg_payload

Field Documentation

§ event_cfg

zb_zcl_device_management_event_cfg_attr_t zb_zcl_device_management_report_event_cfg_payload_s::event_cfg

The configuration bitmap applicable to the event.

See also
zb_zcl_device_management_report_event_cfg_cmd_payload_t::event_cfg_payload

§ event_id

zb_uint16_t zb_zcl_device_management_report_event_cfg_payload_s::event_id

The Event ID is the attribute ID of the Event Configuration attribute.


The documentation for this struct was generated from the following file: