PublishChangeOfSupplier Command Payload Format More...
#include <zb_zcl_device_management.h>
PublishChangeOfSupplier Command Payload Format
| zb_uint32_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::cur_provider_id |
The Current Provider ID field represents a unique identifier for the current commodity provider to whom this command relates.
| zb_uint32_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::implement_time |
The Provider Change Implementation Time field represents a UTC Time to indicate the date/time at which a proposed change to the provider is to be implemented.
| zb_uint32_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::issuer_event_id |
The Issuer Event ID field represents a unique identifier generated by the commodity provider.
| zb_uint8_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::prop_provider_contact_det[ZB_ZCL_DEVICE_MANAGEMENT_PROP_PROVIDER_CONTACT_DET_MAX_SIZE] |
The Proposed Provider Contact Details field represents the contact details of the new commodity provider (see max size below).
| zb_uint32_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::prop_provider_id |
The Proposed Provider ID field represents a unique identifier for the commodity provider associated with the proposed change to the supply.
| zb_uint8_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::prop_provider_name[ZB_ZCL_DEVICE_MANAGEMENT_PROP_PROVIDER_NAME_MAX_SIZE] |
The Proposed Provider Name field represents the name of the new commodity provider (see max size below).
| zb_uint32_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::provider_change_ctrl |
The Provider Change Control field represents the functions that are required to be carried out on processing of this command.
| zb_uint8_t zb_zcl_device_management_publish_change_of_supplier_cmd_payload_s::tariff_type |
The Tariff Type field represents the type of tariff published in this command.