Logo
Developing with ZBOSS for Zigbee
zb_zcl_device_management_get_event_cfg_cmd_payload_s Struct Reference

GetEventConfigurationCommand Payload Format More...

#include <zb_zcl_device_management.h>

Data Fields

zb_uint16_t event_id
 

Detailed Description

GetEventConfigurationCommand Payload Format

See also
SE spec, subclause 10.2.4.6

Field Documentation

§ event_id

zb_uint16_t zb_zcl_device_management_get_event_cfg_cmd_payload_s::event_id

The Event ID field represents particular event to be queried.


The documentation for this struct was generated from the following file: