#include <zb_zcl_daily_schedule.h>
PublishSchedule command
| zb_uint16_t zb_zcl_daily_schedule_publish_schedule_payload_s::day_id |
Unique identifier generated by the commodity supplier.
| zb_uint32_t zb_zcl_daily_schedule_publish_schedule_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.
| zb_uint32_t zb_zcl_daily_schedule_publish_schedule_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
| zb_uint32_t zb_zcl_daily_schedule_publish_schedule_payload_s::schedule_id |
Unique identifier generated by the commodity Supplier to identify a particular schedule.
| zb_uint8_t zb_zcl_daily_schedule_publish_schedule_payload_s::schedule_name[1+12] |
The ScheduleName provides a method for utilities to assign a name to a schedule.
| zb_uint8_t zb_zcl_daily_schedule_publish_schedule_payload_s::schedule_time_reference |
This field indicates how the Start Times contained in the schedule are to be interpreted.
| zb_uint8_t zb_zcl_daily_schedule_publish_schedule_payload_s::schedule_type |
An 8-bit enumeration identifying the type of schedule published in this command.
| zb_uint32_t zb_zcl_daily_schedule_publish_schedule_payload_s::start_time |
A UTC Time field to denote the time at which the published schedule becomes valid. A start date/time of 0x00000000 shall indicate that the command should be executed immediately.