#include <zb_zcl_daily_schedule.h>
PublishDayProfile command payload.
| zb_uint8_t zb_zcl_daily_schedule_publish_day_profile_payload_s::command_index |
The CommandIndex is used to count the payload fragments in the case where the entire payload does not fit into one message. The CommandIndex starts at 0 and is incremented for each fragment belonging to the same command
| zb_uint16_t zb_zcl_daily_schedule_publish_day_profile_payload_s::day_id |
Unique identifier generated by the commodity supplier. The Day ID is used as a reference to assign a Day Profile to a Daily Schedule
| zb_zcl_daily_schedule_entry_t* zb_zcl_daily_schedule_publish_day_profile_payload_s::day_schedule_entries |
day_schedule_entries pointer is considered as a beginning of array (of day schedule entries), number_of_entries_in_this_command - as a number of entries. Please also take into account overall ZCL payload size.
| zb_uint32_t zb_zcl_daily_schedule_publish_day_profile_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.
| zb_uint8_t zb_zcl_daily_schedule_publish_day_profile_payload_s::number_of_entries_in_this_command |
An 8-bit integer representing the number of Day Schedule entries in this command
| zb_uint32_t zb_zcl_daily_schedule_publish_day_profile_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
| zb_uint32_t zb_zcl_daily_schedule_publish_day_profile_payload_s::schedule_id |
Unique identifier generated by the commodity Supplier to identify a particular schedule.
| zb_uint8_t zb_zcl_daily_schedule_publish_day_profile_payload_s::schedule_type |
An 8-bit enumeration identifying the type of schedule published in this command.
| zb_uint8_t zb_zcl_daily_schedule_publish_day_profile_payload_s::total_number_of_commands |
In the case where the entire payload does not fit into one message, the Total Number of Commands field indicates the total number of sub-commands in the message.
| zb_uint8_t zb_zcl_daily_schedule_publish_day_profile_payload_s::total_number_of_schedule_entries |
An 8-bit integer representing the total number of ScheduleEntries in this Day Profile.