Logo
Developing with ZBOSS for Zigbee
zb_zcl_daily_schedule_get_day_profile_payload_s Struct Reference

#include <zb_zcl_daily_schedule.h>

Data Fields

zb_uint32_t provider_id
 
zb_uint16_t day_id
 

Detailed Description

GetDayProfile command payload

See also
Zigbee-17-05035-004, D.9.2.4.2

Field Documentation

§ day_id

zb_uint16_t zb_zcl_daily_schedule_get_day_profile_payload_s::day_id

ScheduleID of the schedule to which the requested Day Profile belongs.

§ provider_id

zb_uint32_t zb_zcl_daily_schedule_get_day_profile_payload_s::provider_id

An unsigned 32-bit field containing a unique identifier for the commodity provider.


The documentation for this struct was generated from the following file: