#include <zb_zcl_daily_schedule.h>
Data Fields | |
| zb_uint32_t | provider_id |
| zb_uint32_t | schedule_id |
| zb_uint8_t | schedule_type |
CancelSchedule command payload.
| zb_uint32_t zb_zcl_daily_schedule_cancel_schedule_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
| zb_uint32_t zb_zcl_daily_schedule_cancel_schedule_payload_s::schedule_id |
Unique identifier generated by the commodity Supplier to identify a particular schedule.
| zb_uint8_t zb_zcl_daily_schedule_cancel_schedule_payload_s::schedule_type |
An 8-bit enumeration identifying the type of schedule published in this command.