Logo
Developing with ZBOSS for Zigbee

#include <zb_zcl_commands.h>

Data Fields

zb_uint8_t status
 
zb_uint8_t direction
 
zb_uint16_t attr_id
 

Detailed Description

One chunk of Configure reporting response command

Attribute status record

Field Documentation

§ attr_id

zb_uint16_t zb_zcl_configure_reporting_res_s::attr_id

Attribute ID

§ direction

zb_uint8_t zb_zcl_configure_reporting_res_s::direction

Direction

§ status

zb_uint8_t zb_zcl_configure_reporting_res_s::status

Configure reporting status


The documentation for this struct was generated from the following file: