Logo
Developing with ZBOSS for Zigbee
zb_zcl_color_control_move_color_req_s Struct Reference

Structure representation of Move Color command payload. More...

#include <zb_zcl_color_control.h>

Data Fields

zb_int16_t rate_x
 
zb_int16_t rate_y
 

Detailed Description

Structure representation of Move Color command payload.

See also
ZCL8 spec, subclause 5.2.2.3.12.1

Field Documentation

§ rate_x

zb_int16_t zb_zcl_color_control_move_color_req_s::rate_x

RateX

§ rate_y

zb_int16_t zb_zcl_color_control_move_color_req_s::rate_y

RateY


The documentation for this struct was generated from the following file: