Logo
Developing with ZBOSS for Zigbee

ZCL attribute definition structure. More...

#include <zb_zcl_common.h>

Data Fields

zb_uint16_t id
 
zb_uint8_t type
 
zb_uint8_t access
 
zb_uint16_t manuf_code
 
void * data_p
 

Detailed Description

ZCL attribute definition structure.

Field Documentation

§ access

zb_uint8_t zb_zcl_attr_s::access

Attribute access options according to zcl_attr_access

§ data_p

void* zb_zcl_attr_s::data_p

Pointer to data

§ id

zb_uint16_t zb_zcl_attr_s::id

Attribute id

§ manuf_code

zb_uint16_t zb_zcl_attr_s::manuf_code

Manufactirer specific ID

§ type

zb_uint8_t zb_zcl_attr_s::type

Attribute type see zcl_attr_type


The documentation for this struct was generated from the following file: