Logo
Developing with ZBOSS for Zigbee
zb_nwk_signal_device_associated_params_s Struct Reference

Association parameters. More...

#include <zboss_api_zdo.h>

Data Fields

zb_ieee_addr_t device_addr
 

Detailed Description

Association parameters.

Stack passes this parameter to application when some device associates to that.

Field Documentation

§ device_addr

zb_ieee_addr_t zb_nwk_signal_device_associated_params_s::device_addr

address of associated device


The documentation for this struct was generated from the following file: