§ index
In the callback function: Index of the returned neighbour table entry. The value of ZB_NWK_NBR_ITERATOR_INDEX_EOT indicates that the entry was not returned and the buffer payload should be ignored. If the structure is passed as the API call parameters: Index, from which the next neighbour table entry should be searched.
§ update_count
| zb_uint32_t zb_nwk_nbr_iterator_cb_params_s::update_count |
In the callback function: The current value of the table update counter. This parameter is ignored in the API call parameters.
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_stable/include/zboss_api_nwk.h