Structure that contains report about any NVRAM failure. Pointer to this structure will be set as additional info in error_app_handler with error code ERROR_CODE(ERROR_CATEGORY_NVRAM, ZB_ERROR_NVRAM_WRITE_VALIDATION_FAILURE). Upon receiving of this error, user can decide what to do: More...
#include <zboss_api.h>
Data Fields | |
| zb_uint32_t | pos |
| zb_uint16_t | ds_type |
| zb_uint8_t | page |
| zb_uint8_t | reserved [1] |
Structure that contains report about any NVRAM failure. Pointer to this structure will be set as additional info in error_app_handler with error code ERROR_CODE(ERROR_CATEGORY_NVRAM, ZB_ERROR_NVRAM_WRITE_VALIDATION_FAILURE). Upon receiving of this error, user can decide what to do:
| zb_uint16_t zb_nvram_failure_report_s::ds_type |
Dataset type
| zb_uint8_t zb_nvram_failure_report_s::page |
Page of dataset payload that haven't been written
| zb_uint32_t zb_nvram_failure_report_s::pos |
Position of dataset payload that haven't been written
| zb_uint8_t zb_nvram_failure_report_s::reserved[1] |
Reserved for future use