Developing with ZBOSS for Zigbee
Data Fields
zb_bdb_signal_touchlink_nwk_joined_router_s Struct Reference
Zigbee stack API
»
Application structure & commissioning start
»
ZBOSS commissioning signals handler
Data Fields
zb_ieee_addr_t
device_ieee_addr
zb_uint8_t
endpoint
zb_uint16_t
profile_id
Field Documentation
§
device_ieee_addr
zb_ieee_addr_t
zb_bdb_signal_touchlink_nwk_joined_router_s::device_ieee_addr
address of device that started the network
The documentation for this struct was generated from the following file:
/conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_stable/include/zboss_api_zdo.h
Copyright (c) 2012-2022 DSR Corporation, Golden CO, USA.
http://www.dsr-zboss.com
http://www.dsr-corporation.com
ZBOSS documentation. Wed Oct 29 2025.