Logo
Developing with ZBOSS for Zigbee
zb_apsme_remove_all_groups_req_s Struct Reference

APSME-REMOVE-ALL-GROUPS.request primitive parameters, should be passed to zb_zdo_remove_all_groups_req(). More...

#include <zboss_api_aps.h>

Data Fields

zb_uint8_t endpoint
 
zb_callback_t confirm_cb
 

Detailed Description

APSME-REMOVE-ALL-GROUPS.request primitive parameters, should be passed to zb_zdo_remove_all_groups_req().

Field Documentation

§ confirm_cb

zb_callback_t zb_apsme_remove_all_groups_req_s::confirm_cb

The callback to be called when the operation is completed.

§ endpoint

zb_uint8_t zb_apsme_remove_all_groups_req_s::endpoint

The endpoint to which the given group is being removed.


The documentation for this struct was generated from the following file: