APSME-ADD-GROUP.confirm primitive parameters. More...
#include <zboss_api_aps.h>
Data Fields | |
| zb_uint16_t | group_address |
| zb_uint8_t | endpoint |
| zb_ret_t | status |
APSME-ADD-GROUP.confirm primitive parameters.
| zb_uint8_t zb_apsme_add_group_conf_s::endpoint |
The endpoint to which the given group is being added.
| zb_uint16_t zb_apsme_add_group_conf_s::group_address |
The 16-bit address of the group being added.
| zb_ret_t zb_apsme_add_group_conf_s::status |
Request send status.