#include <zboss_api_af.h>
Node descriptor
| zb_uint8_t zb_af_node_desc_s::desc_capability_field |
Descriptor capability field
| zb_uint8_t zb_af_node_desc_s::mac_capability_flags |
mac capability
| zb_uint16_t zb_af_node_desc_s::manufacturer_code |
Manufacturer code
| zb_uint8_t zb_af_node_desc_s::max_buf_size |
Maximum buffer size
| zb_uint16_t zb_af_node_desc_s::max_incoming_transfer_size |
Maximum incoming transfer size
| zb_uint16_t zb_af_node_desc_s::max_outgoing_transfer_size |
Maximum outgoing transfer size
| zb_uint16_t zb_af_node_desc_s::node_desc_flags |
node description
| zb_uint16_t zb_af_node_desc_s::server_mask |
Server mask