Data Structures | |
| struct | zb_zcl_default_resp_payload_s |
| Default response payload structure. More... | |
Macros | |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_DIRECTION(buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, seq_num, cmd, status_code, direction) |
| Send default response command with custom Direction. More... | |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_WITH_CB(buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, seq_num, cmd, status_code, callback) |
| Send default response command and execute callback when it is acknowledged or expired. More... | |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_WITH_CB_NEW(buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, seq_num, cmd, status_code, callback, aps_secured) |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_MANUF_WITH_CB(buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, seq_num, cmd, status_code, manuf_code, direction, callback) |
| Send default response command and execute callback when it's acknowledged or expired. More... | |
| #define | ZB_ZCL_CHECK_IF_SEND_DEFAULT_RESP_EXT( _is_broadcast, _delivery_mode, _disable_def_resp, _status, _is_def_resp_frame) |
| check whether command requires default response to be sent More... | |
| #define | ZB_ZCL_CHECK_IF_SEND_DEFAULT_RESP(_cmd_info, _status) |
| API call that is used to check if it is needed to send Default response for the command. More... | |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_EXT(_buffer, _dst_addr, _dst_addr_mode, _dst_ep, _src_ep, _prof_id, _cluster_id, _seq_num, _cmd, _status_code, _direction, _is_manuf_specific, _manuf_code, _callback) |
| General API for sending Default response command. More... | |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_EXT_SECURED(_buffer, _dst_addr, _dst_addr_mode, _dst_ep, _src_ep, _prof_id, _cluster_id, _seq_num, _cmd, _status_code, _direction, _is_manuf_specific, _manuf_code, _callback, _aps_secured) |
| #define | ZB_ZCL_SEND_DEFAULT_RESP(buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, seq_num, cmd, status_code) |
| Send default response command. More... | |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_NEW(buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, seq_num, cmd, status_code, aps_secured) |
| #define | ZB_ZCL_SEND_DEFAULT_RESP_MANUF( buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, seq_num, cmd, status_code, manuf_code, direction) |
| Send default response command. More... | |
| #define | ZB_ZCL_READ_DEFAULT_RESP(buffer) |
| Default response structured reading. More... | |
Typedefs | |
| typedef struct zb_zcl_default_resp_payload_s | zb_zcl_default_resp_payload_t |
| Default response payload structure. | |
Default response command is defined in ZCL spec, subclause 2.4.12.
| #define ZB_ZCL_CHECK_IF_SEND_DEFAULT_RESP | ( | _cmd_info, | |
| _status | |||
| ) |
API call that is used to check if it is needed to send Default response for the command.
| _cmd_info | - variable of zb_zcl_parsed_hdr_t type, containing received command header data |
| _status | - status of the handled command |
| #define ZB_ZCL_CHECK_IF_SEND_DEFAULT_RESP_EXT | ( | _is_broadcast, | |
| _delivery_mode, | |||
| _disable_def_resp, | |||
| _status, | |||
| _is_def_resp_frame | |||
| ) |
check whether command requires default response to be sent
Default response is sent if:
This is a helper method, use ZB_ZCL_CHECK_IF_SEND_DEFAULT_RESP instead
| _is_broadcast | - broadcast bit from NWK header |
| _delivery_mode | - delivery mode from APS header |
| _disable_def_resp | - Disable Default Response bit from ZCL header |
| _status | - status of the handled command |
| _is_def_resp_frame | - check for command type |
| #define ZB_ZCL_READ_DEFAULT_RESP | ( | buffer | ) |
Default response structured reading.
| buffer | - pointer to the message buffer (of type zb_bufid_t) containing payload |
| #define ZB_ZCL_SEND_DEFAULT_RESP | ( | buffer, | |
| addr, | |||
| addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| cluster_id, | |||
| seq_num, | |||
| cmd, | |||
| status_code | |||
| ) |
Send default response command.
| buffer | - ID zb_bufid_t of a buffer with payload |
| addr | - short destination address |
| addr_mode | - address mode, only ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT and ZB_APS_ADDR_MODE_16_ENDP_PRESENT are supported |
| dst_ep | - destination end point |
| ep | - our end point |
| prof_id | - profile identifier |
| cluster_id | - cluster identifier |
| seq_num | - sequence number |
| cmd | - identifier of the command the response is dedicated to |
| status_code | - status field for received command |
| #define ZB_ZCL_SEND_DEFAULT_RESP_DIRECTION | ( | buffer, | |
| addr, | |||
| addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| cluster_id, | |||
| seq_num, | |||
| cmd, | |||
| status_code, | |||
| direction | |||
| ) |
Send default response command with custom Direction.
If you don't want to specify direction explicitly, use ZB_ZCL_SEND_DEFAULT_RESP()
| buffer | - ID zb_bufid_t of a buffer with payload |
| addr | - short destination address |
| addr_mode | - address mode, only ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT and ZB_APS_ADDR_MODE_16_ENDP_PRESENT are supported |
| dst_ep | - destination end point |
| ep | - our end point |
| prof_id | - profile identifier |
| cluster_id | - cluster identifier |
| seq_num | - sequence number |
| cmd | - identifier of the command the response is dedicated to |
| status_code | - status field for received command |
| direction | - direction of the command (see zcl_frame_direction) |
| #define ZB_ZCL_SEND_DEFAULT_RESP_EXT | ( | _buffer, | |
| _dst_addr, | |||
| _dst_addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _prof_id, | |||
| _cluster_id, | |||
| _seq_num, | |||
| _cmd, | |||
| _status_code, | |||
| _direction, | |||
| _is_manuf_specific, | |||
| _manuf_code, | |||
| _callback | |||
| ) |
General API for sending Default response command.
| _buffer | - zb_bufid_t buffer |
| _dst_addr | - 16-bit destination address |
| _dst_addr_mode | - destination address mode. Possible values ZB_APS_ADDR_MODE_DST_ADDR_ENDP_NOT_PRESENT, ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT, ZB_APS_ADDR_MODE_16_ENDP_PRESENT |
| _dst_ep | - destination Endpoint number |
| _src_ep | - source Endpoint number |
| _prof_id | - profile ID |
| _cluster_id | - cluster ID |
| _seq_num | - transaction sequence number |
| _cmd | - command ID |
| _status_code | - command status (see zcl_status) |
| _direction | - direction of command (see zcl_frame_direction) |
| _is_manuf_specific | - flag, equal to 1 if command is manufacturer specific |
| _manuf_code | - manufacturer specific code, is taken unto account only if _is_manuf_specific is equal to 1 |
| _callback | - pointer to the callback function that will be called when the command is sent |
| #define ZB_ZCL_SEND_DEFAULT_RESP_EXT_SECURED | ( | _buffer, | |
| _dst_addr, | |||
| _dst_addr_mode, | |||
| _dst_ep, | |||
| _src_ep, | |||
| _prof_id, | |||
| _cluster_id, | |||
| _seq_num, | |||
| _cmd, | |||
| _status_code, | |||
| _direction, | |||
| _is_manuf_specific, | |||
| _manuf_code, | |||
| _callback, | |||
| _aps_secured | |||
| ) |
| #define ZB_ZCL_SEND_DEFAULT_RESP_MANUF | ( | buffer, | |
| addr, | |||
| addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| cluster_id, | |||
| seq_num, | |||
| cmd, | |||
| status_code, | |||
| manuf_code, | |||
| direction | |||
| ) |
Send default response command.
| buffer | - ID zb_bufid_t of a buffer with payload |
| addr | - short destination address |
| addr_mode | - address mode, only ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT and ZB_APS_ADDR_MODE_16_ENDP_PRESENT are supported |
| dst_ep | - destination end point |
| ep | - our end point |
| prof_id | - profile identifier |
| cluster_id | - cluster identifier |
| seq_num | - sequence number |
| cmd | - identifier of the command the response is dedicated to |
| status_code | - status field for received command |
| manuf_code | - manufacturer code |
| direction | - direction of command (see zcl_frame_direction) |
| #define ZB_ZCL_SEND_DEFAULT_RESP_MANUF_WITH_CB | ( | buffer, | |
| addr, | |||
| addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| cluster_id, | |||
| seq_num, | |||
| cmd, | |||
| status_code, | |||
| manuf_code, | |||
| direction, | |||
| callback | |||
| ) |
Send default response command and execute callback when it's acknowledged or expired.
If no callback is needed, use ZB_ZCL_SEND_DEFAULT_RESP()
| buffer | - ID zb_bufid_t of a buffer with payload |
| addr | - short destination address |
| addr_mode | - address mode, only ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT and ZB_APS_ADDR_MODE_16_ENDP_PRESENT are supported |
| dst_ep | - destination end point |
| ep | - our end point |
| prof_id | - profile identifier |
| cluster_id | - cluster identifier |
| seq_num | - sequence number |
| cmd | - identifier of the command the response is dedicated to |
| status_code | - status field for received command |
| manuf_code | - manufacturer code |
| direction | - direction of the command (see zcl_frame_direction) |
| callback | - callback to be executed when command is acknowledged or expired (of type zb_callback_t) |
| #define ZB_ZCL_SEND_DEFAULT_RESP_NEW | ( | buffer, | |
| addr, | |||
| addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| cluster_id, | |||
| seq_num, | |||
| cmd, | |||
| status_code, | |||
| aps_secured | |||
| ) |
| #define ZB_ZCL_SEND_DEFAULT_RESP_WITH_CB | ( | buffer, | |
| addr, | |||
| addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| cluster_id, | |||
| seq_num, | |||
| cmd, | |||
| status_code, | |||
| callback | |||
| ) |
Send default response command and execute callback when it is acknowledged or expired.
If no callback is needed, use ZB_ZCL_SEND_DEFAULT_RESP()
| buffer | - ID zb_bufid_t of a buffer with payload |
| addr | - short destination address |
| addr_mode | - address mode, only ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT and ZB_APS_ADDR_MODE_16_ENDP_PRESENT are supported |
| dst_ep | - destination end point |
| ep | - our end point |
| prof_id | - profile identifier |
| cluster_id | - cluster identifier |
| seq_num | - sequence number |
| cmd | - identifier of the command the response is dedicated to |
| status_code | - status field for received command |
| callback | - callback to be executed when command is acknowledged or expired (of type zb_callback_t) |
| #define ZB_ZCL_SEND_DEFAULT_RESP_WITH_CB_NEW | ( | buffer, | |
| addr, | |||
| addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prof_id, | |||
| cluster_id, | |||
| seq_num, | |||
| cmd, | |||
| status_code, | |||
| callback, | |||
| aps_secured | |||
| ) |