Macros | |
| #define | ZB_BDB_COMM_ACTIVE_ENDP_LIST_LEN 4 |
| #define | BDB_MAX_IDENTIFY_QUERY_RESP_NUMBER 4 |
Typedefs | |
| typedef enum zb_bdb_comm_state_e | zb_bdb_comm_state_t |
Enumerations | |
| enum | zb_bdb_comm_state_e { ZB_BDB_COMM_IDLE = 0, ZB_BDB_COMM_FINDING_AND_BINDING = 4, ZB_BDB_COMM_FINDING_AND_BINDING_TARGET = 5 } |
Functions | |
| void | zb_set_bdb_primary_channel_set (zb_uint32_t channel_mask) |
| zb_uint32_t | zb_get_bdb_primary_channel_set (void) |
| void | zb_set_bdb_secondary_channel_set (zb_uint32_t channel_mask) |
| zb_uint32_t | zb_get_bdb_secondary_channel_set (void) |
| void | zb_bdb_set_legacy_device_support (zb_uint8_t state) |
| #define BDB_MAX_IDENTIFY_QUERY_RESP_NUMBER 4 |
Identify query responses queue size
| #define ZB_BDB_COMM_ACTIVE_ENDP_LIST_LEN 4 |
Maximum endpoints of the "respondent" that can be served
| typedef enum zb_bdb_comm_state_e zb_bdb_comm_state_t |
List of BDB commissioning states
| enum zb_bdb_comm_state_e |
| void zb_bdb_set_legacy_device_support | ( | zb_uint8_t | state | ) |
Enable Zigbee PRO complaint commissioning support
| state | - 1 to disable trust center require key exchange; 0 - to enable. |
| zb_uint32_t zb_get_bdb_primary_channel_set | ( | void | ) |
Get the primary channel set for the BDB energy scan.
| zb_uint32_t zb_get_bdb_secondary_channel_set | ( | void | ) |
Get the secondary channel set for the BDB energy scan.
| void zb_set_bdb_primary_channel_set | ( | zb_uint32_t | channel_mask | ) |
Set the primary channel set for the BDB energy scan. Beacon request will be send on these channels
| channel_mask | - Channel mask. |
| void zb_set_bdb_secondary_channel_set | ( | zb_uint32_t | channel_mask | ) |
Set the secondary channel set for the BDB energy scan. Beacon request will be send on these channels if no network found after energy scan on the primary channels.
| channel_mask | - Channel mask. |