Macros | |
| #define | ZB_JOINED() zb_zdo_joined() |
Functions | |
| zb_bool_t | zb_get_rx_on_when_idle (void) |
| const zb_char_t ZB_IAR_CODE * | zb_get_version (void) |
| Get ZBOSS version. More... | |
| zb_uint32_t | zboss_version_get (void) |
| Get ZBOSS numeric version. More... | |
| void | zb_get_long_address (zb_ieee_addr_t addr) |
| zb_uint16_t | zb_get_pan_id (void) |
| zb_uint16_t | zb_get_short_address (void) |
| void | zb_get_extended_pan_id (zb_ext_pan_id_t ext_pan_id) |
| zb_uint8_t | zb_get_current_page (void) |
| zb_uint8_t | zb_get_current_channel (void) |
| zb_nwk_device_type_t | zb_get_network_role (void) |
| zb_uint8_t | zb_get_max_children (void) |
| #define ZB_JOINED | ( | ) | zb_zdo_joined() |
Checks that device is joined to the network.
| zb_uint8_t zb_get_current_channel | ( | void | ) |
Get the currently used channel.
| zb_uint8_t zb_get_current_page | ( | void | ) |
Get the currently used channel page.
| void zb_get_extended_pan_id | ( | zb_ext_pan_id_t | ext_pan_id | ) |
Get Extended Pan ID (nwkExtendedPANId attribute)
| ext_pan_id | - pointer to memory where result will be stored |
| void zb_get_long_address | ( | zb_ieee_addr_t | addr | ) |
Get 64-bit long address
| addr | - pointer to memory where result will be stored |
| zb_uint8_t zb_get_max_children | ( | void | ) |
Returns the maximum number of children allowed
| zb_nwk_device_type_t zb_get_network_role | ( | void | ) |
Returns the device role ID
| zb_uint16_t zb_get_pan_id | ( | void | ) |
Get 16-bit PAN ID
| zb_bool_t zb_get_rx_on_when_idle | ( | void | ) |
Returns current state of RX-ON-When-Idle of Zigbee ZED
| zb_uint16_t zb_get_short_address | ( | void | ) |
Get current short address of the device
| const zb_char_t ZB_IAR_CODE* zb_get_version | ( | void | ) |
Get ZBOSS version.
| zb_uint32_t zboss_version_get | ( | void | ) |
Get ZBOSS numeric version.