Enable Concentrator mode for the device (disabled by default). It's possible to call this function to send MTORR immediately, e.g. after a new device joined the network. It does affect only for Coordinator role.
- Parameters
-
| radius | - the hop count radius for concentrator route discoveries. If the value is set zero then the default radius will be used. |
| disc_time | - the time in seconds between concentrator route discoveries. If the value is set to zero, the route discoveries are done by the application layer only. |