Macros | |
| #define | RET_OK 0 |
| Error codes for non-void stack functions. In general, function can return OK, BLOCKED or some error. Errors are negative. More... | |
| #define | RET_ERROR ERROR_CODE(ERROR_CATEGORY_GENERIC, 1) /* -1 indeed */ |
| #define | RET_BLOCKED ERROR_CODE(ERROR_CATEGORY_GENERIC, 2) |
| #define | RET_EXIT ERROR_CODE(ERROR_CATEGORY_GENERIC, 3) |
| #define | RET_BUSY ERROR_CODE(ERROR_CATEGORY_GENERIC, 4) |
| #define | RET_EOF ERROR_CODE(ERROR_CATEGORY_GENERIC, 5) |
| #define | RET_OUT_OF_RANGE ERROR_CODE(ERROR_CATEGORY_GENERIC, 6) |
| #define | RET_EMPTY ERROR_CODE(ERROR_CATEGORY_GENERIC, 7) |
| #define | RET_CANCELLED ERROR_CODE(ERROR_CATEGORY_GENERIC, 8) |
| #define | RET_INVALID_PARAMETER_1 ERROR_CODE(ERROR_CATEGORY_GENERIC, 10) |
| #define | RET_INVALID_PARAMETER_2 ERROR_CODE(ERROR_CATEGORY_GENERIC, 11) |
| #define | RET_INVALID_PARAMETER_3 ERROR_CODE(ERROR_CATEGORY_GENERIC, 12) |
| #define | RET_INVALID_PARAMETER_4 ERROR_CODE(ERROR_CATEGORY_GENERIC, 13) |
| #define | RET_INVALID_PARAMETER_6 ERROR_CODE(ERROR_CATEGORY_GENERIC, 15) |
| #define | RET_PENDING ERROR_CODE(ERROR_CATEGORY_GENERIC, 21) |
| #define | RET_NO_MEMORY ERROR_CODE(ERROR_CATEGORY_GENERIC, 22) |
| #define | RET_INVALID_PARAMETER ERROR_CODE(ERROR_CATEGORY_GENERIC, 23) |
| #define | RET_OPERATION_FAILED ERROR_CODE(ERROR_CATEGORY_GENERIC, 24) |
| #define | RET_BUFFER_TOO_SMALL ERROR_CODE(ERROR_CATEGORY_GENERIC, 25) |
| #define | RET_END_OF_LIST ERROR_CODE(ERROR_CATEGORY_GENERIC, 26) |
| #define | RET_ALREADY_EXISTS ERROR_CODE(ERROR_CATEGORY_GENERIC, 27) |
| #define | RET_NOT_FOUND ERROR_CODE(ERROR_CATEGORY_GENERIC, 28) |
| #define | RET_OVERFLOW ERROR_CODE(ERROR_CATEGORY_GENERIC, 29) |
| #define | RET_TIMEOUT ERROR_CODE(ERROR_CATEGORY_GENERIC, 30) |
| #define | RET_NOT_IMPLEMENTED ERROR_CODE(ERROR_CATEGORY_GENERIC, 31) |
| #define | RET_NO_RESOURCES ERROR_CODE(ERROR_CATEGORY_GENERIC, 32) |
| #define | RET_UNINITIALIZED ERROR_CODE(ERROR_CATEGORY_GENERIC, 33) |
| #define | RET_INVALID_STATE ERROR_CODE(ERROR_CATEGORY_GENERIC, 35) |
| #define | RET_CONNECTION_FAILED ERROR_CODE(ERROR_CATEGORY_GENERIC, 37) |
| #define | RET_CONNECTION_LOST ERROR_CODE(ERROR_CATEGORY_GENERIC, 38) |
| #define | RET_UNAUTHORIZED ERROR_CODE(ERROR_CATEGORY_GENERIC, 40) |
| #define | RET_CONFLICT ERROR_CODE(ERROR_CATEGORY_GENERIC, 41) |
| #define | RET_INVALID_FORMAT ERROR_CODE(ERROR_CATEGORY_GENERIC, 42) |
| #define | RET_NO_MATCH ERROR_CODE(ERROR_CATEGORY_GENERIC, 43) |
| #define | RET_PROTOCOL_ERROR ERROR_CODE(ERROR_CATEGORY_GENERIC, 44) |
| #define | RET_VERSION ERROR_CODE(ERROR_CATEGORY_GENERIC, 45) |
| #define | RET_FILE_NOT_FOUND ERROR_CODE(ERROR_CATEGORY_GENERIC, 48) |
| #define | RET_CONVERSION_ERROR ERROR_CODE(ERROR_CATEGORY_GENERIC, 50) |
| #define | RET_FILE_CORRUPTED ERROR_CODE(ERROR_CATEGORY_GENERIC, 56) |
| #define | RET_PAGE_NOT_FOUND ERROR_CODE(ERROR_CATEGORY_GENERIC, 57) |
| #define | RET_ILLEGAL_REQUEST ERROR_CODE(ERROR_CATEGORY_GENERIC, 62) |
| #define | RET_INVALID_GROUP ERROR_CODE(ERROR_CATEGORY_GENERIC, 64) |
| #define | RET_TABLE_FULL ERROR_CODE(ERROR_CATEGORY_GENERIC, 65) |
| #define | RET_IGNORE ERROR_CODE(ERROR_CATEGORY_GENERIC, 69) |
| #define | RET_AGAIN ERROR_CODE(ERROR_CATEGORY_GENERIC, 70) |
| #define | RET_DEVICE_NOT_FOUND ERROR_CODE(ERROR_CATEGORY_GENERIC, 71) |
| #define | RET_OBSOLETE ERROR_CODE(ERROR_CATEGORY_GENERIC, 72) |
| #define | RET_INTERRUPTED ERROR_CODE(ERROR_CATEGORY_GENERIC, 73) |
| #define | RET_NULL_POINTER ERROR_CODE(ERROR_CATEGORY_GENERIC, 74) |
| #define RET_OK 0 |
Error codes for non-void stack functions. In general, function can return OK, BLOCKED or some error. Errors are negative.
Error can be "generic" or some additional error code.