Macros | |
| #define | ZB_MIN_ENDPOINT_NUMBER 1U |
| Minimum valid endpoint number. | |
| #define | ZB_MAX_ENDPOINT_NUMBER 240U |
| Maximum valid endpoint number. | |
| #define | ZB_APS_BROADCAST_ENDPOINT_NUMBER 255U |
| Broadcast endpoint number. | |
Typedefs | |
| typedef zb_uint8_t | zb_aps_status_t |
| Type for APS status constants. More... | |
| typedef zb_uint8_t | zb_aps_addr_mode_t |
| Type for APS addressing mode constants. More... | |
APS status constants | |
| #define | ZB_APS_STATUS_SUCCESS 0x00U |
| #define | ZB_APS_ASDU_TOO_LONG 0xa0U |
| #define | ZB_APS_DEFRAG_DEFERRED 0xa1U |
| #define | ZB_APS_DEFRAG_UNSUPPORTED 0xa2U |
| #define | ZB_APS_STATUS_ILLEGAL_REQUEST 0xa3U |
| #define | ZB_APS_STATUS_INVALID_BINDING 0xa4U |
| #define | ZB_APS_STATUS_INVALID_GROUP 0xa5U |
| #define | ZB_APS_STATUS_INVALID_PARAMETER 0xa6U |
| #define | ZB_APS_STATUS_NO_ACK 0xa7U |
| #define | ZB_APS_STATUS_NO_BOUND_DEVICE 0xa8U |
| #define | ZB_APS_STATUS_NO_SHORT_ADDRESS 0xa9U |
| #define | ZB_APS_STATUS_NOT_SUPPORTED 0xaaU |
| #define | ZB_APS_STATUS_SECURED_LINK_KEY 0xabU |
| #define | ZB_APS_STATUS_SECURED_NWK_KEY 0xacU |
| #define | ZB_APS_STATUS_SECURITY_FAIL 0xadU |
| #define | ZB_APS_STATUS_TABLE_FULL 0xaeU |
| #define | ZB_APS_STATUS_UNSECURED 0xafU |
| #define | ZB_APS_STATUS_UNSUPPORTED_ATTRIBUTE 0xb0U |
APS addressing mode constants | |
| #define | ZB_APS_ADDR_MODE_DST_ADDR_ENDP_NOT_PRESENT 0x00U |
| #define | ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT 0x01U |
| #define | ZB_APS_ADDR_MODE_16_ENDP_PRESENT 0x02U |
| #define | ZB_APS_ADDR_MODE_64_ENDP_PRESENT 0x03U |
| #define | ZB_APS_ADDR_MODE_BIND_TBL_ID 0x04U |
| #define ZB_APS_ADDR_MODE_16_ENDP_PRESENT 0x02U |
16-bit address for DstAddress and DstEndpoint present
| #define ZB_APS_ADDR_MODE_16_GROUP_ENDP_NOT_PRESENT 0x01U |
16-bit group address for DstAddress; DstEndpoint not present
| #define ZB_APS_ADDR_MODE_64_ENDP_PRESENT 0x03U |
64-bit extended address for DstAddress and DstEndpoint present
| #define ZB_APS_ADDR_MODE_BIND_TBL_ID 0x04U |
"destination endpoint" is interpreted as an index in the binding table, all other destination address information is ignored
| #define ZB_APS_ADDR_MODE_DST_ADDR_ENDP_NOT_PRESENT 0x00U |
DstAddress and DstEndpoint not present
| #define ZB_APS_ASDU_TOO_LONG 0xa0U |
A transmit request failed since the ASDU is too large and fragmentation is not supported.
| #define ZB_APS_DEFRAG_DEFERRED 0xa1U |
A received fragmented frame could not be defragmented at the current time.
| #define ZB_APS_DEFRAG_UNSUPPORTED 0xa2U |
A received fragmented frame could not be defragmented since the device does not support fragmentation.
| #define ZB_APS_STATUS_ILLEGAL_REQUEST 0xa3U |
A parameter value was out of range.
| #define ZB_APS_STATUS_INVALID_BINDING 0xa4U |
An APSME-UNBIND.request failed due to the requested binding link not existing in the binding table.
| #define ZB_APS_STATUS_INVALID_GROUP 0xa5U |
An APSME-REMOVE-GROUP.request has been issued with a group identifier that does not appear in the group table.
| #define ZB_APS_STATUS_INVALID_PARAMETER 0xa6U |
A parameter value was invalid or out of range.
| #define ZB_APS_STATUS_NO_ACK 0xa7U |
An APSDE-DATA.request requesting acknowledged transmission failed due to no acknowledgement being received.
| #define ZB_APS_STATUS_NO_BOUND_DEVICE 0xa8U |
An APSDE-DATA.request with a destination addressing mode set to 0x00 failed due to there being no devices bound to this device.
| #define ZB_APS_STATUS_NO_SHORT_ADDRESS 0xa9U |
An APSDE-DATA.request with a destination addressing mode set to 0x03 failed due to no corresponding short address found in the address map table.
| #define ZB_APS_STATUS_NOT_SUPPORTED 0xaaU |
An APSDE-DATA.request with a destination addressing mode set to 0x00 failed due to a binding table not being supported on the device.
| #define ZB_APS_STATUS_SECURED_LINK_KEY 0xabU |
An ASDU was received that was secured using a link key.
| #define ZB_APS_STATUS_SECURED_NWK_KEY 0xacU |
An ASDU was received that was secured using a network key.
| #define ZB_APS_STATUS_SECURITY_FAIL 0xadU |
An APSDE-DATA.request requesting security has resulted in an error during the corresponding security processing.
| #define ZB_APS_STATUS_SUCCESS 0x00U |
A request has been executed successfully.
| #define ZB_APS_STATUS_TABLE_FULL 0xaeU |
An APSME-BIND.request or APSME.ADD-GROUP.request issued when the binding or group tables, respectively, were full.
| #define ZB_APS_STATUS_UNSECURED 0xafU |
An ASDU was received without any security.
| #define ZB_APS_STATUS_UNSUPPORTED_ATTRIBUTE 0xb0U |
An APSME-GET.request or APSME-SET.request has been issued with an unknown attribute identifier.
| typedef zb_uint8_t zb_aps_addr_mode_t |
Type for APS addressing mode constants.
Holds one of aps_addr_mode. Kept only for backward compatibility as aps_addr_mode were declared previously as enum.
| typedef zb_uint8_t zb_aps_status_t |
Type for APS status constants.