WWAH cluster attribute identifiers.
| Enumerator |
|---|
| ZB_ZCL_ATTR_WWAH_DISABLE_OTA_DOWNGRADES_ID | If set to TRUE, the device SHALL disallow downgrades of it's firmware.
|
| ZB_ZCL_ATTR_WWAH_MGMT_LEAVE_WITHOUT_REJOIN_ENABLED_ID | If set to FALSE, the node SHALL ignore MGMT Leave Without Rejoin commands.
|
| ZB_ZCL_ATTR_WWAH_NWK_RETRY_COUNT_ID | This attribute is a fixed value containing the number of Network Level Retries the device performs when sending a unicast command, not including APS retries.
|
| ZB_ZCL_ATTR_WWAH_MAC_RETRY_COUNT_ID | This attribute is a fixed value containing the number of MAC Level Retries the device performs when sending a unicast command, not including APS retries.
|
| ZB_ZCL_ATTR_WWAH_ROUTER_CHECK_IN_ENABLED_ID | This attribute is set to TRUE if the router's check-in algorithm has been enabled through the 'Enable Periodic Router Check-Ins' command detailed below.
|
| ZB_ZCL_ATTR_WWAH_TOUCHLINK_INTERPAN_ENABLED_ID | This attribute is set to FALSE if support for Touchlink Interpan messages has been disabled on the device.
|
| ZB_ZCL_ATTR_WWAH_WWAH_PARENT_CLASSIFICATION_ENABLED_ID | If set to TRUE, the device SHALL enable the WWAH Parent Classification Advertisements feature.
|
| ZB_ZCL_ATTR_WWAH_WWAH_APP_EVENT_RETRY_ENABLED_ID | This attribute is TRUE if the WWAH Application Event Retry Algorithm is enabled.
|
| ZB_ZCL_ATTR_WWAH_WWAH_APP_EVENT_RETRY_QUEUE_SIZE_ID | This attribute is the queue size for re-delivery attempts in the WWAH Application Event Retry Algorithm.
|
| ZB_ZCL_ATTR_WWAH_WWAH_REJOIN_ENABLED_ID | This attribute is set to TRUE if the WWAH Rejoin Algorithm is enabled.
|
| ZB_ZCL_ATTR_WWAH_MAC_POLL_FAILURE_WAIT_TIME_ID | This attribute is the time in seconds the device waits before retrying a data poll when a MAC level data poll fails for any reason.
|
| ZB_ZCL_ATTR_WWAH_CONFIGURATION_MODE_ENABLED_ID | This attribute indicates whether the device is able to be configured using ZDO commands that are not encrypted using the Trust Center Link Key.
|
| ZB_ZCL_ATTR_WWAH_CURRENT_DEBUG_REPORT_ID_ID | This attribute contains the ID of the current debug report stored on the node.
|
| ZB_ZCL_ATTR_WWAH_TC_SECURITY_ON_NWK_KEY_ROTATION_ENABLED_ID | If this attribute is set to TRUE, the node SHALL only process network key rotation commands which are sent via unicast and are encrypted by the Trust Center Link Key.
|
| ZB_ZCL_ATTR_WWAH_WWAH_BAD_PARENT_RECOVERY_ENABLED_ID | If this attribute is set to TRUE, the endpoint device SHALL enable the WWAH Bad Parent Recovery feature.
|
| ZB_ZCL_ATTR_WWAH_PENDING_NETWORK_UPDATE_CHANNEL_ID | This attribute contains the channel number of the only channel the device SHALL accept in a ZDO Mgmt Network Update command.
|
| ZB_ZCL_ATTR_WWAH_PENDING_NETWORK_UPDATE_PANID_ID | This attribute contains the only short PAN ID the device SHALL accept in a NLME Network Update command.
|
| ZB_ZCL_ATTR_WWAH_OTA_MAX_OFFLINE_DURATION_ID | This attribute contains the maximum time in seconds the device may be unavailable after completing its OTA download (while restarting, etc).
|