Modules | |
| WWAH cluster attributes | |
| WWAH cluster commands | |
This cluster provides an opportunity to use various features of the Work With All Hubs cluster.
The WWAH cluster shall exist on only 1 endpoint of the Zigbee node, it should be identified using cluster ID 0xfc57 and manufacturer ID 0x1217.
All configurations/command settings in this cluster shall be persisted across power cycles and rejoins. Only a device factory reset can reset this cluster and put it back to default settings.
For more information see Zigbee WWAH Cluster definition (document number in Zigbee Alliance 17-01067-022).