Tariff Information (Delivered) Attributes Set.
| Enumerator |
|---|
| ZB_ZCL_ATTR_PRICE_SRV_TARIFF_LABEL | The TariffLabel attribute provides a method for utilities to assign a label to an entire set of tariff information.
|
| ZB_ZCL_ATTR_PRICE_SRV_NUMBER_OF_PRICE_TIERS_IN_USE | An 8-bit integer which indicates the number of price tiers used while this tariff is active.
|
| ZB_ZCL_ATTR_PRICE_SRV_NUMBER_OF_BLOCK_THRESHOLDS_IN_USE | An 8-bit integer which indicates the total number of block thresholds used in the currently active tariff.
|
| ZB_ZCL_ATTR_PRICE_SRV_TIER_BLOCK_MODE | An 8-bit enumeration indicating how the mixed TOU / Block charging is to be applied.
|
| ZB_ZCL_ATTR_PRICE_SRV_UNIT_OF_MEASURE | An 8-bit enumeration identifying the base unit of measure.
|
| ZB_ZCL_ATTR_PRICE_SRV_CURRENCY | An unsigned 16-bit integer containing identifying information concerning the local unit of currency used in the Price cluster.
|
| ZB_ZCL_ATTR_PRICE_SRV_PRICE_TRAILING_DIGIT | An 8-bit BitMap used to determine where the decimal point is located for prices provided in the Standing Charge attribute and the Price Matrix command.
|
| ZB_ZCL_ATTR_PRICE_SRV_TARIFF_RESOLUTION_PERIOD | An 8-bit enumeration identifying the resolution period for Block Tariff.
|
| ZB_ZCL_ATTR_PRICE_SRV_CO2 | Used to calculate the amount of carbon dioxide (CO2) produced from energy use.
|
| ZB_ZCL_ATTR_PRICE_SRV_CO2_UNIT | This attribute is an 8-bit enumeration which defines the unit for the CO2 attribute.
|
| ZB_ZCL_ATTR_PRICE_SRV_CO2_TRAILING_DIGIT | An 8-bit Bit-Map used to determine where the decimal point is located in the CO2 attribute.
|