Logo
Developing with ZBOSS for Zigbee

Enumerations

enum  zb_zcl_price_set_received_block_threshold_e {
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK1_THRESHOLD = ZB_ZCL_ATTR_SET_WITH_ATTR_ID(ZB_ZCL_PRICE_SET_RECEIVED_BLOCK_THRESHOLD, 0x00), ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK2_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK3_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK4_THRESHOLD,
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK5_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK6_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK7_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK8_THRESHOLD,
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK9_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK10_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK11_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK12_THRESHOLD,
  ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK13_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK14_THRESHOLD, ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK15_THRESHOLD
}
 Received Block Threshold Attributes Set. More...
 

Detailed Description

This set of attributes provides remote access to the Price server ReceivedBlockThresholds. The number of block thresholds is indicated by the NumberOfBlockThresholds field in the associated PublishTariffInformation command. The number of blocks is one greater than the number of thresholds.

Enumeration Type Documentation

§ zb_zcl_price_set_received_block_threshold_e

Received Block Threshold Attributes Set.

See also
SE spec, D.4.2.2.11
Enumerator
ZB_ZCL_ATTR_PRICE_SRV_RECEIVED_BLOCK1_THRESHOLD 

The format of these attributes is the same as for the 'Delivered' Block Thresholds