Logo
Developing with ZBOSS for Zigbee
ZB_ZCL_MULTISTATE_VALUE

Data Structures

struct  zb_zcl_multi_value_attrs_s
 Multistate Value cluster attributes. More...
 

Macros

#define ZB_ZCL_MULTI_VALUE_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0001u)
 Default value for Multistate Value cluster revision global attribute.
 
#define ZB_ZCL_MULTI_VALUE_DESCRIPTION_DEFAULT_VALUE   {0}
 Default value for Description attribute.
 
#define ZB_ZCL_MULTI_VALUE_OUT_OF_SERVICE_DEFAULT_VALUE   ZB_FALSE
 Default value for OutOfService attribute.
 
#define ZB_ZCL_MULTI_VALUE_RELIABILITY_DEFAULT_VALUE   ZB_ZCL_MULTI_VALUE_RELIABILITY_NO_FAULT_DETECTED
 Default value for Reliability attribute.
 
#define ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_DEFAULT_VALUE   ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_NORMAL
 Default value for StatusFlags attribute.
 
#define ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_MIN_VALUE   0
 StatusFlags attribute minimum value.
 
#define ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_MAX_VALUE   0x0f
 StatusFlags attribute maximum value.
 
#define ZB_ZCL_DECLARE_MULTI_VALUE_ATTRIB_LIST(attr_list, description, out_of_service, present_value, reliability, relinquish_default, status_flags, app_type)
 Declare attribute list for Multistate Value cluster. More...
 
#define ZB_ZCL_MULTI_VALUE_DESCRIPTION_MAX_LEN   16
 
#define ZB_ZCL_DECLARE_MULTI_VALUE_ATTR_LIST(attr_list, attrs)
 Declare attribute list for Multistate Value cluster. More...
 

Typedefs

typedef struct zb_zcl_multi_value_attrs_s zb_zcl_multi_value_attrs_t
 Multistate Value cluster attributes.
 

Multistate Value cluster attributes

enum  zb_zcl_multi_value_attr_e {
  ZB_ZCL_ATTR_MULTI_VALUE_DESCRIPTION_ID = 0x001c, ZB_ZCL_ATTR_MULTI_VALUE_OUT_OF_SERVICE_ID = 0x0051, ZB_ZCL_ATTR_MULTI_VALUE_PRESENT_VALUE_ID = 0x0055, ZB_ZCL_ATTR_MULTI_VALUE_RELIABILITY_ID = 0x0067,
  ZB_ZCL_ATTR_MULTI_VALUE_RELINQUISH_DEFAULT_ID = 0x0068, ZB_ZCL_ATTR_MULTI_VALUE_STATUS_FLAGS_ID = 0x006f, ZB_ZCL_ATTR_MULTI_VALUE_APPLICATION_TYPE_ID = 0x0100
}
 Multistate Value cluster attribute identifiers. More...
 
enum  zb_zcl_multi_value_status_flags_value_e {
  ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_NORMAL = 0x00, ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_IN_ALARM = 0x01, ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_FAULT = 0x02, ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_OVERRIDDEN = 0x04,
  ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_OUT_OF_SERVICE = 0x08
}
 StatusFlags attribute values. More...
 
enum  zb_zcl_multi_value_reliability_value_e {
  ZB_ZCL_MULTI_VALUE_RELIABILITY_NO_FAULT_DETECTED = 0x00, ZB_ZCL_MULTI_VALUE_RELIABILITY_NO_SENSOR = 0x01, ZB_ZCL_MULTI_VALUE_RELIABILITY_OVER_RANGE = 0x02, ZB_ZCL_MULTI_VALUE_RELIABILITY_UNDER_RANGE = 0x03,
  ZB_ZCL_MULTI_VALUE_RELIABILITY_OPEN_LOOP = 0x04, ZB_ZCL_MULTI_VALUE_RELIABILITY_SHORTED_LOOP = 0x05, ZB_ZCL_MULTI_VALUE_RELIABILITY_NO_OUTPUT = 0x06, ZB_ZCL_MULTI_VALUE_RELIABILITY_UNRELIABLE_OTHER = 0x07,
  ZB_ZCL_MULTI_VALUE_RELIABILITY_PROCESS_ERROR = 0x08, ZB_ZCL_MULTI_VALUE_RELIABILITY_MULTI_STATE_FAULT = 0x09, ZB_ZCL_MULTI_VALUE_RELIABILITY_CONFIGURATION_ERROR = 0x0a
}
 Reliability attribute values. More...
 

Multistate Value cluster application types

The ApplicationType attribute indicates the specific application usage for the cluster. ApplicationType is subdivided into Group, Type and an Index number, as follows:

  • Group = Bits 24 to 31 An indication of the cluster this attribute is part of. Multistate Value clusters have Group = 0x0d.
  • Type = Bits 16 to 23 The physical quantity that the PresentValue attribute of the cluster represents.
  • Index = Bits 0 to 15 The specific application usage of the cluster.
enum  zb_zcl_mv_application_types_e { ZB_ZCL_MV_APP_TYPE_APP_DOMAIN_HVAC = 0x0000 }
 Type values for Multistate Value cluster applications. More...
 
enum  zb_zcl_mv_app_domain_hvac_e {
  ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_0 = ZB_ZCL_MV_SET_APP_TYPE_WITH_ID(ZB_ZCL_MV_APP_TYPE_APP_DOMAIN_HVAC, 0x0000), ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_1, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_2, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_3,
  ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_4, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_5, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_6, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_7,
  ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_8, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_9, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_10, ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_11,
  ZB_ZCL_MV_APP_DOMAIN_HVAC_OTHER = ZB_ZCL_MV_SET_APP_TYPE_WITH_ID(ZB_ZCL_MV_APP_TYPE_APP_DOMAIN_HVAC, 0xffff)
}
 
#define ZB_ZCL_MV_GROUP_ID   0x0d
 
#define ZB_ZCL_MV_SET_APP_TYPE_WITH_ID(_type, _id)   ((ZB_ZCL_MV_GROUP_ID << 24) | ((_type & 0xff) << 16) | (_id & 0xffff))
 

Detailed Description

The Multistate Value (Basic) cluster provides an interface for setting a multistate value, typically used as a control system parameter, and accessing characteristics of that value.

Macro Definition Documentation

§ ZB_ZCL_DECLARE_MULTI_VALUE_ATTR_LIST

#define ZB_ZCL_DECLARE_MULTI_VALUE_ATTR_LIST (   attr_list,
  attrs 
)
Value:
&attrs.description, \
&attrs.out_of_service, \
&attrs.present_value, \
&attrs.reliability, \
&attrs.relinquish_default, \
&attrs.status_flags, \
&attrs.application_type)
#define ZB_ZCL_DECLARE_MULTI_VALUE_ATTRIB_LIST(attr_list, description, out_of_service, present_value, reliability, relinquish_default, status_flags, app_type)
Declare attribute list for Multistate Value cluster.
Definition: zb_zcl_multistate_value.h:290

Declare attribute list for Multistate Value cluster.

Parameters
[in]attr_list- attribute list variable name
[in]attrs- variable of zb_zcl_multi_value_attrs_t type (containing Multistate Value cluster attributes)

§ ZB_ZCL_DECLARE_MULTI_VALUE_ATTRIB_LIST

#define ZB_ZCL_DECLARE_MULTI_VALUE_ATTRIB_LIST (   attr_list,
  description,
  out_of_service,
  present_value,
  reliability,
  relinquish_default,
  status_flags,
  app_type 
)
Value:
\
ZB_ZCL_START_DECLARE_ATTRIB_LIST_CLUSTER_REVISION(attr_list, ZB_ZCL_MULTI_VALUE) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_MULTI_VALUE_DESCRIPTION_ID, (description)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_MULTI_VALUE_OUT_OF_SERVICE_ID, (out_of_service)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_MULTI_VALUE_PRESENT_VALUE_ID, (present_value)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_MULTI_VALUE_RELIABILITY_ID, (reliability)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_MULTI_VALUE_RELINQUISH_DEFAULT_ID, (relinquish_default)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_MULTI_VALUE_STATUS_FLAGS_ID, (status_flags)) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_MULTI_VALUE_APPLICATION_TYPE_ID, (app_type)) \
ZB_ZCL_FINISH_DECLARE_ATTRIB_LIST
PriorityArray attribute, ZCL spec 3.14.11.6.
Definition: zb_zcl_multistate_value.h:72
OutOfService attribute, ZCL spec 3.14.11.1.
Definition: zb_zcl_multistate_value.h:63
ApplicationType attribute, ZCL spec 3.14.11.19.
Definition: zb_zcl_multistate_value.h:78
StatusFlags attribute, ZCL spec 3.14.11.3.
Definition: zb_zcl_multistate_value.h:76
PresentValue attribute, ZCL spec 3.14.11.2.
Definition: zb_zcl_multistate_value.h:65
Reliability attribute, ZCL spec 3.14.11.7.
Definition: zb_zcl_multistate_value.h:74
Description attribute, ZCL spec 3.14.11.4.
Definition: zb_zcl_multistate_value.h:56

Declare attribute list for Multistate Value cluster.

Parameters
attr_list- attribute list name
description- pointer to variable storing Description attribute value
out_of_service- pointer to variable storing OutOfService attribute value
present_value- pointer to variable storing PresentValue attribute value
reliability- pointer to variable storing Reliability attribute value
relinquish_default- pointer to variable storing RelinquishDefault attribute value
status_flags- pointer to variable storing StatusFlags attribute value
app_type- pointer to variable storing ApplicationType attribute value

§ ZB_ZCL_MULTI_VALUE_DESCRIPTION_MAX_LEN

#define ZB_ZCL_MULTI_VALUE_DESCRIPTION_MAX_LEN   16

Maximum length of Description string field

Enumeration Type Documentation

§ zb_zcl_multi_value_attr_e

Multistate Value cluster attribute identifiers.

See also
ZCL spec, Multistate Value (Basic) Cluster 3.14.4.4.2
Enumerator
ZB_ZCL_ATTR_MULTI_VALUE_DESCRIPTION_ID 

Description attribute, ZCL spec 3.14.11.4.

ZB_ZCL_ATTR_MULTI_VALUE_OUT_OF_SERVICE_ID 

OutOfService attribute, ZCL spec 3.14.11.1.

ZB_ZCL_ATTR_MULTI_VALUE_PRESENT_VALUE_ID 

PresentValue attribute, ZCL spec 3.14.11.2.

ZB_ZCL_ATTR_MULTI_VALUE_RELIABILITY_ID 

PriorityArray attribute, ZCL spec 3.14.11.6.

Reliability attribute, ZCL spec 3.14.11.9

ZB_ZCL_ATTR_MULTI_VALUE_RELINQUISH_DEFAULT_ID 

Reliability attribute, ZCL spec 3.14.11.7.

ZB_ZCL_ATTR_MULTI_VALUE_STATUS_FLAGS_ID 

StatusFlags attribute, ZCL spec 3.14.11.3.

ZB_ZCL_ATTR_MULTI_VALUE_APPLICATION_TYPE_ID 

ApplicationType attribute, ZCL spec 3.14.11.19.

§ zb_zcl_multi_value_reliability_value_e

Reliability attribute values.

See also
ZCL spec 3.14.11.9 for details.
Enumerator
ZB_ZCL_MULTI_VALUE_RELIABILITY_NO_FAULT_DETECTED 

No fault detected

ZB_ZCL_MULTI_VALUE_RELIABILITY_NO_SENSOR 

No sensor

ZB_ZCL_MULTI_VALUE_RELIABILITY_OVER_RANGE 

Over range

ZB_ZCL_MULTI_VALUE_RELIABILITY_UNDER_RANGE 

Under range

ZB_ZCL_MULTI_VALUE_RELIABILITY_OPEN_LOOP 

Open loop

ZB_ZCL_MULTI_VALUE_RELIABILITY_SHORTED_LOOP 

Shorted loop

ZB_ZCL_MULTI_VALUE_RELIABILITY_NO_OUTPUT 

No output

ZB_ZCL_MULTI_VALUE_RELIABILITY_UNRELIABLE_OTHER 

Unreliable other

ZB_ZCL_MULTI_VALUE_RELIABILITY_PROCESS_ERROR 

Process error

ZB_ZCL_MULTI_VALUE_RELIABILITY_MULTI_STATE_FAULT 

Mutlistate fault

ZB_ZCL_MULTI_VALUE_RELIABILITY_CONFIGURATION_ERROR 

Configuration error

§ zb_zcl_multi_value_status_flags_value_e

StatusFlags attribute values.

See also
ZCL spec 3.14.11.3 for details.
Enumerator
ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_NORMAL 

Normal (default) .

ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_IN_ALARM 

In alarm bit.

ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_FAULT 

Fault bit.

ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_OVERRIDDEN 

Overridden bit.

ZB_ZCL_MULTI_VALUE_STATUS_FLAGS_OUT_OF_SERVICE 

Out of service bit.

§ zb_zcl_mv_app_domain_hvac_e

Enumerator
ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_0 

On, Off, Auto state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_1 

Off, Low, Medium, High state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_2 

Auto, Heat, Cool, Off, Emergency Heat, Fan Only, Max Heat state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_3 

Occupied, Unoccupied, Standby, Bypass state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_4 

Inactive, Active, Hold state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_5 

Auto, Warm-up, Water Flush, Autocalibration, Shutdown Open, Shutdown Closed, Low Limit, Test and Balance state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_6 

Off, Auto, Heat Control, Heat Only, Cool Only, Fan Only state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_7 

High, Normal, Low state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_8 

Occupied, Unoccupied, Startup, Shutdown state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_9 

Night, Day, Hold state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_10 

Off, Cool, Heat, Auto, Emergency Heat state

ZB_ZCL_MV_APP_DOMAIN_HVAC_STATES_GROUP_11 

Shutdown Closed, Shutdown Open, Satisfied, Mixing, Cooling, Heating, Supplemental Heat state

ZB_ZCL_MV_APP_DOMAIN_HVAC_OTHER 

Other

§ zb_zcl_mv_application_types_e

Type values for Multistate Value cluster applications.

See also
ZCL spec 3.16.11.19.9
Enumerator
ZB_ZCL_MV_APP_TYPE_APP_DOMAIN_HVAC 

Application Domain HVAC