Logo
Developing with ZBOSS for Zigbee
Remove Group command definitions

Data Structures

struct  zb_zcl_groups_remove_group_req_s
 Remove Group command structure. More...
 
struct  zb_zcl_groups_remove_group_res_s
 Remove group response command structure. More...
 

Macros

#define ZB_ZCL_GROUPS_GET_REMOVE_GROUP_REQ(data_buf, rem_group_req)
 Parses Remove group command and fills in data request structure. If request contains invalid data, ZB_ZCL_NULL_ID is stored as group_id. More...
 
#define ZB_ZCL_GROUPS_GET_REMOVE_GROUP_RES(data_buf, rem_group_res)
 Parses Remove group response command and returns response data structure or NULL if request contains invalid data. More...
 
#define ZB_ZCL_GROUPS_SEND_REMOVE_GROUP_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, group_id)
 Send Remove group command. More...
 

Typedefs

typedef struct zb_zcl_groups_remove_group_req_s zb_zcl_groups_remove_group_req_t
 Remove Group command structure.
 
typedef struct zb_zcl_groups_remove_group_res_s zb_zcl_groups_remove_group_res_t
 Remove group response command structure.
 

Detailed Description

Remove Group request and response commands have simple payload. Actual request handling takes place in ZCL internals.

Examples
Remove Group request sending:
ZB_ZCL_GROUPS_SEND_REMOVE_GROUP_REQ(buffer, DST_ADDR, DST_ADDR_MODE, ENDPOINT_C, ENDPOINT_ED, ZB_AF_HA_PROFILE_ID, ZB_ZCL_ENABLE_DEFAULT_RESPONSE, NULL, TEST_GROUP_ID_2);

Macro Definition Documentation

§ ZB_ZCL_GROUPS_GET_REMOVE_GROUP_REQ

#define ZB_ZCL_GROUPS_GET_REMOVE_GROUP_REQ (   data_buf,
  rem_group_req 
)
Value:
{ \
zb_zcl_groups_remove_group_req_t *rem_group_req_ptr; \
(rem_group_req_ptr) = zb_buf_len(data_buf) >= ZB_ZCL_REMOVE_GROUP_REQ_SIZE ? \
\
if (rem_group_req_ptr) \
{ \
ZB_HTOLE16(&(rem_group_req).group_id, &rem_group_req_ptr->group_id); \
} \
else \
{ \
rem_group_req.group_id = ZB_ZCL_NULL_ID; \
} \
}
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:344
Remove Group command structure.
Definition: zb_zcl_groups.h:536
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:362

Parses Remove group command and fills in data request structure. If request contains invalid data, ZB_ZCL_NULL_ID is stored as group_id.

Parameters
data_buf- pointer to zb_buf_t buffer containing command request data
rem_group_req- variable to save command request
Note
data_buf buffer should contain command request payload without ZCL header.

§ ZB_ZCL_GROUPS_GET_REMOVE_GROUP_RES

#define ZB_ZCL_GROUPS_GET_REMOVE_GROUP_RES (   data_buf,
  rem_group_res 
)
Value:
{ \
(rem_group_res) = zb_buf_len(data_buf) >= ZB_ZCL_REMOVE_GROUP_RES_SIZE ? \
\
if (rem_group_res) \
{ \
ZB_ZCL_HTOLE16_INPLACE(&(rem_group_res)->group_id); \
} \
}
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:344
Remove group response command structure.
Definition: zb_zcl_groups.h:573
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:362

Parses Remove group response command and returns response data structure or NULL if request contains invalid data.

Parameters
data_buf- pointer to zb_buf_t buffer containing command response data
rem_group_res- out pointer to zb_zcl_groups_remove_group_res_t, containing command response record
Note
data_buf buffer should contain response command payload without ZCL header

§ ZB_ZCL_GROUPS_SEND_REMOVE_GROUP_REQ

#define ZB_ZCL_GROUPS_SEND_REMOVE_GROUP_REQ (   buffer,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  def_resp,
  cb,
  group_id 
)
Value:
{ \
zb_uint8_t* ptr = ZB_ZCL_START_PACKET_REQ(buffer) \
ZB_ZCL_CONSTRUCT_SPECIFIC_COMMAND_REQ_FRAME_CONTROL(ptr, def_resp) \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_REQ(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_GROUPS_REMOVE_GROUP); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (group_id)); \
ZB_ZCL_FINISH_PACKET(buffer, ptr) \
ZB_ZCL_SEND_COMMAND_SHORT( \
buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, ZB_ZCL_CLUSTER_ID_GROUPS, cb); \
}
#define ZB_ZCL_CLUSTER_ID_GROUPS
Definition: zb_zcl_common.h:211
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1463
Definition: zb_zcl_groups.h:94

Send Remove group command.

Parameters
bufferto put packet to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
def_resp- enable/disable default response
cb- callback for getting command send status
group_id- group ID to remove