Logo
Developing with ZBOSS for Zigbee
ZCL Groups cluster

Modules

 Add group command definitions
 
 View group command definitions
 
 Get Group Membership command definitions
 
 Remove Group command definitions
 
 Remove All Groups command definitions
 
 Add group if identifying command definitions
 

Functions

zb_bool_t zb_zcl_process_groups_commands_srv (zb_uint8_t param)
 
zb_bool_t zb_zcl_process_groups_commands_cli (zb_uint8_t param)
 

Groups cluster attributes

enum  zb_zcl_groups_attr_e { ZB_ZCL_ATTR_GROUPS_NAME_SUPPORT_ID = 0 }
 Groups cluster attribute identifiers. More...
 
enum  zb_zcl_groups_name_support_e { ZB_ZCL_ATTR_GROUPS_NAME_NOT_SUPPORTED = 0, ZB_ZCL_ATTR_GROUPS_NAME_SUPPORTED = 1 << 7 }
 Values for NameSupport attribute. More...
 
#define ZB_ZCL_GROUPS_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0003u)
 Default value for Groups cluster revision global attribute.
 
#define ZB_ZCL_DECLARE_GROUPS_ATTRIB_LIST(attr_list, name_support)
 Declare attribute list for Groups cluster. More...
 

Groups cluster command identifiers

enum  zb_zcl_groups_cmd_e {
  ZB_ZCL_CMD_GROUPS_ADD_GROUP = 0x00, ZB_ZCL_CMD_GROUPS_VIEW_GROUP = 0x01, ZB_ZCL_CMD_GROUPS_GET_GROUP_MEMBERSHIP = 0x02, ZB_ZCL_CMD_GROUPS_REMOVE_GROUP = 0x03,
  ZB_ZCL_CMD_GROUPS_REMOVE_ALL_GROUPS = 0x04, ZB_ZCL_CMD_GROUPS_ADD_GROUP_IF_IDENTIFYING = 0x05
}
 Groups cluster command identifiers. More...
 
enum  zb_zcl_groups_cmd_resp_e { ZB_ZCL_CMD_GROUPS_ADD_GROUP_RES = 0x00, ZB_ZCL_CMD_GROUPS_VIEW_GROUP_RES = 0x01, ZB_ZCL_CMD_GROUPS_GET_GROUP_MEMBERSHIP_RES = 0x02, ZB_ZCL_CMD_GROUPS_REMOVE_GROUP_RES = 0x03 }
 Groups cluster response command identifiers. More...
 

Detailed Description

Groups cluster defined in ZCL spec, clause 3.6. Currently no group name attribute support is implemented. However, this attribute must be supported for sending and receiving in commands' payload, so it is being sent as zero string (i. e. single zero byte). On receipt of the command is able to contain a scene name in the payload, this field will be ignored as a string.

Cluster requests and responses are documented in submodules.

Macro Definition Documentation

§ ZB_ZCL_DECLARE_GROUPS_ATTRIB_LIST

#define ZB_ZCL_DECLARE_GROUPS_ATTRIB_LIST (   attr_list,
  name_support 
)
Value:
ZB_ZCL_START_DECLARE_ATTRIB_LIST_CLUSTER_REVISION(attr_list, ZB_ZCL_GROUPS) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_GROUPS_NAME_SUPPORT_ID, (name_support)) \
ZB_ZCL_FINISH_DECLARE_ATTRIB_LIST
NameSupport attribute.
Definition: zb_zcl_groups.h:53

Declare attribute list for Groups cluster.

Parameters
attr_list- attribute list name.
name_support- pointer to variable to store name_support attribute value

Enumeration Type Documentation

§ zb_zcl_groups_attr_e

Groups cluster attribute identifiers.

See also
ZCL spec, subclause 3.6.2.2
Enumerator
ZB_ZCL_ATTR_GROUPS_NAME_SUPPORT_ID 

NameSupport attribute.

§ zb_zcl_groups_cmd_e

Groups cluster command identifiers.

See also
ZCL spec, subclause 3.6.2.2.2.
Enumerator
ZB_ZCL_CMD_GROUPS_ADD_GROUP 

Add group command identifier.

ZB_ZCL_CMD_GROUPS_VIEW_GROUP 

View group command identifier.

ZB_ZCL_CMD_GROUPS_GET_GROUP_MEMBERSHIP 

Get group membership command identifier.

ZB_ZCL_CMD_GROUPS_REMOVE_GROUP 

Remove group command identifier.

ZB_ZCL_CMD_GROUPS_REMOVE_ALL_GROUPS 

Remove all groups command identifier.

ZB_ZCL_CMD_GROUPS_ADD_GROUP_IF_IDENTIFYING 

Add group if identifying command identifier.

§ zb_zcl_groups_cmd_resp_e

Groups cluster response command identifiers.

See also
ZCL spec, subclause 3.6.2.3
Enumerator
ZB_ZCL_CMD_GROUPS_ADD_GROUP_RES 

Add group response command identifier.

ZB_ZCL_CMD_GROUPS_VIEW_GROUP_RES 

View group response command identifier.

ZB_ZCL_CMD_GROUPS_GET_GROUP_MEMBERSHIP_RES 

Get group response membership command identifier.

ZB_ZCL_CMD_GROUPS_REMOVE_GROUP_RES 

Remove group response command identifier.

§ zb_zcl_groups_name_support_e

Values for NameSupport attribute.

Enumerator
ZB_ZCL_ATTR_GROUPS_NAME_NOT_SUPPORTED 

"Not supported" value

ZB_ZCL_ATTR_GROUPS_NAME_SUPPORTED 

"On" value

Function Documentation

§ zb_zcl_process_groups_commands_cli()

zb_bool_t zb_zcl_process_groups_commands_cli ( zb_uint8_t  param)

Handler for incoming group commands directed to client

Parameters
param- reference to buffer containing command
Returns
ZB_TRUE - if command was processed ZB_FALSE - if command is not for client or is not supported

§ zb_zcl_process_groups_commands_srv()

zb_bool_t zb_zcl_process_groups_commands_srv ( zb_uint8_t  param)

Handler for incoming group commands directed to server

Parameters
param- reference to buffer containing command
Returns
ZB_TRUE - if command was processed ZB_FALSE - if command is not for server or is not supported