Data Structures | |
| struct | zb_af_node_desc_s |
| struct | zb_af_node_power_desc_s |
| struct | zb_af_simple_desc_1_1_s |
| struct | zb_af_simple_desc_8_9_s |
| struct | zb_af_endpoint_desc_s |
| Endpoint descriptor. More... | |
Macros | |
| #define | ZB_COORDINATOR ZB_NWK_DEVICE_TYPE_COORDINATOR |
| #define | ZB_ROUTER ZB_NWK_DEVICE_TYPE_ROUTER |
| #define | ZB_END_DEVICE ZB_NWK_DEVICE_TYPE_ED |
| #define | ZB_AF_SIMPLE_DESC_TYPE(in_num, out_num) CAT5(zb_af_simple_desc_,in_num,_,out_num,_t) |
| #define | ZB_DECLARE_SIMPLE_DESC(in_clusters_count, out_clusters_count) |
| #define | ZB_AF_IS_EP_REGISTERED(_ep) ((zb_af_get_endpoint_desc( _ep ) != NULL)?(ZB_TRUE):(ZB_FALSE)) |
| Check endpoint registration in ZCL. More... | |
| #define | ZB_AF_START_DECLARE_ENDPOINT_LIST(ep_list_name) zb_af_endpoint_desc_t *ep_list_name[] = { |
| #define | ZB_AF_DECLARE_ENDPOINT_DESC( ep_name, ep_id, profile_id, reserved_length, reserved_ptr, cluster_number, cluster_list, simple_desc, rep_count, rep_ctx, lev_ctrl_count, lev_ctrl_ctx) |
| Initialize endpoint descriptor. More... | |
| #define | ZB_AF_FINISH_DECLARE_ENDPOINT_LIST } |
| #define | ZB_AF_SET_ENDPOINT_HANDLER(endpoint, handler) (zb_af_get_endpoint_desc((endpoint))->device_handler = (handler)) |
| Allows application to register cluster commands handler for a specific endpoint. More... | |
| #define | ZB_AF_SET_IDENTIFY_NOTIFICATION_HANDLER(endpoint, handler) (zb_af_get_endpoint_desc((endpoint))->identify_handler = (handler)) |
| Sets identify notification handler for endpoint. More... | |
| #define | ZB_ZCL_CLUSTER_DESC(cluster_id, attr_count, attr_desc_list, cluster_role_mask, manuf_code) |
| #define | ZB_AF_DECLARE_DEVICE_CTX(device_ctx_name, ep_list_name, ep_count, reporting_attr_count) |
| #define | ZB_AF_DECLARE_DEVICE_CTX_NO_REP(device_ctx_name, ep_list_name, ep_count) |
| #define | ZBOSS_DEVICE_DECLARE_REPORTING_CTX(rep_ctx, rep_count) zb_zcl_reporting_info_t rep_ctx[rep_count] |
| #define | ZBOSS_DEVICE_DECLARE_LEVEL_CONTROL_CTX(lev_ctrl_ctx, lev_ctrl_count) zb_zcl_cvc_alarm_variables_t lev_ctrl_ctx[lev_ctrl_count] |
| #define | ZBOSS_DECLARE_DEVICE_CTX(device_ctx_name, ep_list_name, ep_count) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_1_EP(device_ctx_name, ep_name) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_2_EP(device_ctx_name, ep1_name, ep2_name) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_3_EP(device_ctx_name, ep1_name, ep2_name, ep3_name) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_4_EP(device_ctx_name, ep1_name, ep2_name, ep3_name, ep4_name) |
| #define | ZB_AF_REGISTER_DEVICE_CTX(_device_ctx) zb_af_register_device_ctx(_device_ctx) |
| #define | ZB_ZCL_REGISTER_DEVICE_CB(func_ptr) |
| Set Device user application callback. The macro sets a callback being called upon to need inform User App about change device attribute or need to execute H/W command. More... | |
Node descriptor - frequency value | |
| #define | ZB_FREQ_BAND_868 1U |
| #define | ZB_FREQ_BAND_SUB_GHZ_NA_FSK (1U << 2) |
| #define | ZB_FREQ_BAND_2400 (1U << 3) |
| #define | ZB_FREQ_BAND_SUB_GHZ_EU_FSK (1U << 4) |
Node descriptor - server mask | |
| #define | ZB_PRIMARY_TRUST_CENTER 1U |
| #define | ZB_BACKUP_TRUST_CENTER (1U << 1) |
| #define | ZB_PRIMARY_BINDING_TABLE_CENTER (1U << 2) |
| #define | ZB_BACKUP_BINDING_TABLE_CENTER (1U << 3) |
| #define | ZB_PRIMARY_DISCOVERY_CACHE (1U << 4) |
| #define | ZB_BACKUP_DISCOVERY_CACHE (1U << 5) |
| #define | ZB_NETWORK_MANAGER (1U << 6) |
Node descriptor - capability mask | |
| #define | ZB_EXT_ACTIVE_EP_LIST 1U |
| #define | ZB_EXT_SIMPLE_DESC_LIST (1U << 1) |
Power descriptor types | |
| #define | ZB_POWER_MODE_SYNC_ON_WHEN_IDLE 0U |
| #define | ZB_POWER_MODE_COME_ON_PERIODICALLY 1U |
| #define | ZB_POWER_MODE_COME_ON_WHEN_STIMULATED 2U |
Power source types | |
| #define | ZB_POWER_SRC_CONSTANT 1U |
| #define | ZB_POWER_SRC_RECHARGEABLE_BATTERY (1U << 1) |
| #define | ZB_POWER_SRC_DISPOSABLE_BATTERY (1U << 2) |
Power source level values | |
| #define | ZB_POWER_LEVEL_CRITICAL 0U |
| #define | ZB_POWER_LEVEL_33 4U |
| #define | ZB_POWER_LEVEL_66 8U |
| #define | ZB_POWER_LEVEL_100 12U |
Profile identifiers | |
| #define | ZB_AF_ZDO_PROFILE_ID 0x0000U |
| #define | ZB_AF_LEGACY_PROFILE1_ID 0x0101U |
| #define | ZB_AF_LEGACY_PROFILE2_ID 0x0102U |
| #define | ZB_AF_LEGACY_PROFILE3_ID 0x0103U |
| #define | ZB_AF_HA_PROFILE_ID 0x0104U |
| #define | ZB_AF_LEGACY_PROFILE4_ID 0x0105U |
| #define | ZB_AF_LEGACY_PROFILE5_ID 0x0106U |
| #define | ZB_AF_LEGACY_PROFILE6_ID 0x0107U |
| #define | ZB_AF_LEGACY_PROFILE7_ID 0x0108U |
| #define | ZB_AF_SE_PROFILE_ID 0x0109U |
| #define | ZB_AF_ZLL_PROFILE_ID 0xC05EU |
| #define | ZB_AF_TEST_PROFILE_ID 0x7F01U |
| #define | ZB_AF_WILDCARD_PROFILE_ID 0xFFFFU |
| #define | ZB_AF_GP_PROFILE_ID 0xA1E0U |
| #define | ZB_MSP_INITIAL_PROFILE_ID 0xC000U |
Typedefs | |
| typedef struct zb_af_node_desc_s | zb_af_node_desc_t |
| typedef zb_nwk_device_type_t | zb_logical_type_t |
| typedef zb_uint8_t | zb_current_power_mode_t |
| Type for power descriptor types. More... | |
| typedef zb_uint8_t | zb_power_src_t |
| Type for power source types. More... | |
| typedef zb_uint8_t | zb_power_source_level_t |
| Type for power source level values. More... | |
| typedef struct zb_af_node_power_desc_s | zb_af_node_power_desc_t |
| typedef struct zb_af_simple_desc_1_1_s | zb_af_simple_desc_1_1_t |
| typedef struct zb_af_simple_desc_8_9_s | zb_af_simple_desc_8_9_t |
| typedef zb_uint8_t(* | zb_device_handler_t) (zb_uint8_t param) |
| typedef struct zb_af_endpoint_desc_s | zb_af_endpoint_desc_t |
| Endpoint descriptor. More... | |
| typedef void(* | zb_af_transmission_res_cb_t) (zb_uint8_t status) |
Functions | |
| zb_af_endpoint_desc_t * | zb_af_get_endpoint_desc (zb_uint8_t ep_id) |
| Search for endpoint (device) descriptor by endpoint ID. More... | |
| void | zb_apsde_data_indication_cont (zb_uint8_t param) |