Logo
Developing with ZBOSS for Zigbee
zb_errors.h File Reference

Macros

#define RET_OK   0
 Error codes for non-void stack functions. In general, function can return OK, BLOCKED or some error. Errors are negative. More...
 
#define RET_ERROR   ERROR_CODE(ERROR_CATEGORY_GENERIC, 1) /* -1 indeed */
 
#define RET_BLOCKED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 2)
 
#define RET_EXIT   ERROR_CODE(ERROR_CATEGORY_GENERIC, 3)
 
#define RET_BUSY   ERROR_CODE(ERROR_CATEGORY_GENERIC, 4)
 
#define RET_EOF   ERROR_CODE(ERROR_CATEGORY_GENERIC, 5)
 
#define RET_OUT_OF_RANGE   ERROR_CODE(ERROR_CATEGORY_GENERIC, 6)
 
#define RET_EMPTY   ERROR_CODE(ERROR_CATEGORY_GENERIC, 7)
 
#define RET_CANCELLED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 8)
 
#define RET_INVALID_PARAMETER_1   ERROR_CODE(ERROR_CATEGORY_GENERIC, 10)
 
#define RET_INVALID_PARAMETER_2   ERROR_CODE(ERROR_CATEGORY_GENERIC, 11)
 
#define RET_INVALID_PARAMETER_3   ERROR_CODE(ERROR_CATEGORY_GENERIC, 12)
 
#define RET_INVALID_PARAMETER_4   ERROR_CODE(ERROR_CATEGORY_GENERIC, 13)
 
#define RET_INVALID_PARAMETER_6   ERROR_CODE(ERROR_CATEGORY_GENERIC, 15)
 
#define RET_PENDING   ERROR_CODE(ERROR_CATEGORY_GENERIC, 21)
 
#define RET_NO_MEMORY   ERROR_CODE(ERROR_CATEGORY_GENERIC, 22)
 
#define RET_INVALID_PARAMETER   ERROR_CODE(ERROR_CATEGORY_GENERIC, 23)
 
#define RET_OPERATION_FAILED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 24)
 
#define RET_BUFFER_TOO_SMALL   ERROR_CODE(ERROR_CATEGORY_GENERIC, 25)
 
#define RET_END_OF_LIST   ERROR_CODE(ERROR_CATEGORY_GENERIC, 26)
 
#define RET_ALREADY_EXISTS   ERROR_CODE(ERROR_CATEGORY_GENERIC, 27)
 
#define RET_NOT_FOUND   ERROR_CODE(ERROR_CATEGORY_GENERIC, 28)
 
#define RET_OVERFLOW   ERROR_CODE(ERROR_CATEGORY_GENERIC, 29)
 
#define RET_TIMEOUT   ERROR_CODE(ERROR_CATEGORY_GENERIC, 30)
 
#define RET_NOT_IMPLEMENTED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 31)
 
#define RET_NO_RESOURCES   ERROR_CODE(ERROR_CATEGORY_GENERIC, 32)
 
#define RET_UNINITIALIZED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 33)
 
#define RET_INVALID_STATE   ERROR_CODE(ERROR_CATEGORY_GENERIC, 35)
 
#define RET_CONNECTION_FAILED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 37)
 
#define RET_CONNECTION_LOST   ERROR_CODE(ERROR_CATEGORY_GENERIC, 38)
 
#define RET_UNAUTHORIZED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 40)
 
#define RET_CONFLICT   ERROR_CODE(ERROR_CATEGORY_GENERIC, 41)
 
#define RET_INVALID_FORMAT   ERROR_CODE(ERROR_CATEGORY_GENERIC, 42)
 
#define RET_NO_MATCH   ERROR_CODE(ERROR_CATEGORY_GENERIC, 43)
 
#define RET_PROTOCOL_ERROR   ERROR_CODE(ERROR_CATEGORY_GENERIC, 44)
 
#define RET_VERSION   ERROR_CODE(ERROR_CATEGORY_GENERIC, 45)
 
#define RET_FILE_NOT_FOUND   ERROR_CODE(ERROR_CATEGORY_GENERIC, 48)
 
#define RET_CONVERSION_ERROR   ERROR_CODE(ERROR_CATEGORY_GENERIC, 50)
 
#define RET_FILE_CORRUPTED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 56)
 
#define RET_PAGE_NOT_FOUND   ERROR_CODE(ERROR_CATEGORY_GENERIC, 57)
 
#define RET_ILLEGAL_REQUEST   ERROR_CODE(ERROR_CATEGORY_GENERIC, 62)
 
#define RET_INVALID_GROUP   ERROR_CODE(ERROR_CATEGORY_GENERIC, 64)
 
#define RET_TABLE_FULL   ERROR_CODE(ERROR_CATEGORY_GENERIC, 65)
 
#define RET_IGNORE   ERROR_CODE(ERROR_CATEGORY_GENERIC, 69)
 
#define RET_AGAIN   ERROR_CODE(ERROR_CATEGORY_GENERIC, 70)
 
#define RET_DEVICE_NOT_FOUND   ERROR_CODE(ERROR_CATEGORY_GENERIC, 71)
 
#define RET_OBSOLETE   ERROR_CODE(ERROR_CATEGORY_GENERIC, 72)
 
#define RET_INTERRUPTED   ERROR_CODE(ERROR_CATEGORY_GENERIC, 73)
 
#define RET_NULL_POINTER   ERROR_CODE(ERROR_CATEGORY_GENERIC, 74)
 
#define RET_CONFIGURATION_ERROR   ERROR_CODE(ERROR_CATEGORY_GENERIC, 75)
 

Typedefs

typedef zb_int32_t zb_ret_t
 Return type for ZB functions returning execution status. More...