#include <zboss_api_zgp.h>
§ addr_ref
§ device_id
§ endpoint
Endpoint pair of IEEE:EP if App ID is 010.
§ ext_options
§ groupcast_radius
To limit the range of the groupcast
§ ieee_addr
Extension to the table (field is not presented in specification).
Dest IEEE address to use in GPT to GPD packets even if GPD is identified by SrcID
§ is_sink
§ lwsaddr
| struct { ... } ::zgp_proxy_tbl_ent_s::zgp_lwsink_addr_list_s zgp_tbl_ent_s::lwsaddr[ 2U ] |
§ match_dev_tbl_idx
index in matching table matched by device_id or app_info.manuf_model_id
§ options
The options for the reception from ZGPD
§ proxy
| struct { ... } ::zgp_proxy_tbl_ent_s zgp_tbl_ent_s::proxy |
§ sec_options
§ security_counter
The incoming security frame counter for ZGPD
§ sgrp
§ sink
| struct { ... } ::zgp_sink_tbl_ent_s zgp_tbl_ent_s::sink |
| union { ... } zgp_tbl_ent_s::u |
§ zgpd_assigned_alias
The commissioned 16-bit ID to be used as alias for ZGPD
§ zgpd_id
§ zgpd_key
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zboss_api_zgp.h