Logo
Developing with ZBOSS for Zigbee
zgp_attr_record_s Struct Reference

#include <zboss_api_zgp.h>

Data Fields

zb_uint16_t id
 
zb_uint8_t data_type
 
zb_uint8_t options
 
zb_uint8_t offset
 
zb_uint8_t value [8U]
 

Field Documentation

§ data_type

zb_uint8_t zgp_attr_record_s::data_type

§ id

zb_uint16_t zgp_attr_record_s::id

§ offset

zb_uint8_t zgp_attr_record_s::offset

§ options

zb_uint8_t zgp_attr_record_s::options

§ value

zb_uint8_t zgp_attr_record_s::value[8U]

The documentation for this struct was generated from the following file: