Commissioning Service request parameters. More...
#include <zboss_api_direct.h>
Data Fields | |
| zb_uint32_t | param_mask |
| Parameter mask (used bits 0 to 16) - indicates what parameters of the request should be considered - zbd_zvd_comm_service_param_bitmasks_t. More... | |
| zb_uint8_t | ext_pan_id [8] |
| [00] Specifies the Zigbee network's extended PAN ID - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_TZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_EXT_PAN_ID More... | |
| zb_uint16_t | short_pan_id |
| [01] Specifies the Zigbee network's short PAN ID - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_SHORT_PAN_ID More... | |
| zbd_nwk_channel_list_t | nwk_channel_list |
| [02] Network Channel List - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_CHANNEL More... | |
| zb_uint8_t | nwk_key [16] |
| [03] Specifies the Zigbee Network Key - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_KEY More... | |
| zb_uint8_t | link_key [16] |
| [04] Specifies the Zigbee Link Key - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_LINK_KEY More... | |
| zb_nwk_device_type_t | device_type |
| [05] Specifies the ZDD's Zigbee device type - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_DEVICE_TYPE More... | |
| zb_uint16_t | nwk_addr |
| [06] Specifies the ZDD's 16-bit Zigbee network address - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_ADDR More... | |
| zb_uint8_t | joining_method |
| [07] Specifies the method the ZDD is instructed to use to join the network - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_JOINING_METHOD More... | |
| zb_uint8_t | ieee_addr [8] |
| [08] The 64-bit IEEE address of the ZDD - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_IEEE_ADDR More... | |
| zb_uint8_t | tc_addr [8] |
| [09] The 64-bit IEEE address of the Trust Center - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_TC_ADDR More... | |
| zbd_network_status_t | nwk_status_map |
| [10] Contains a bitmap that indicates the ZDD's network status - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_STATUS_MAP More... | |
| zb_uint8_t | nwk_update_id |
| [11] Current value of the nwkUpdateId attribute of the Zigbee NIB - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_UPDATE_ID More... | |
| zb_uint8_t | nwk_active_key_seq_num |
| [12] Current value of the nwkActiveKeySeqNumber attribute of the Zigbee NIB - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_ACTIVE_KEY_SEQ_NUM More... | |
| zb_uint8_t | admin_key [16] |
| [13] Specifies the 128-bit Admin Key - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_ADMIN_KEY More... | |
| zbd_status_code_t | status_code |
| [14] Status codes as described in section 7.7.2.4.6 - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_STATUS_CODE , zbd_status_code_s More... | |
| zb_uint8_t | manage_joiners_cmd |
| [15] Manage Joiners Command, as described in section 7.7.2.4.7 - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_MANAGE_JOINERS_CMD , see zbd_manage_joiners_cmd_e More... | |
| zb_uint8_t | manage_joiners_ieee [8] |
| [16] The 64-bit IEEE address of the joiner ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_MANAGE_JOINERS_IEEE , see zbd_manage_joiners_cmd_e More... | |
| zb_uint8_t | manage_joiners_lnk_key [16] |
| [17] Specifies the Zigbee Link Key associated with the joiner ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_MANAGE_JOINERS_LNK_KEY , see zbd_manage_joiners_cmd_e More... | |
| zb_uint8_t | link_key_flags_mask |
| [18] Link Key flags zbd_aps_link_key_flags_mask_t More... | |
Commissioning Service request parameters.
| zb_uint8_t zbd_zvd_comm_service_params_t::admin_key[16] |
[13] Specifies the 128-bit Admin Key - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_ADMIN_KEY
| zb_nwk_device_type_t zbd_zvd_comm_service_params_t::device_type |
[05] Specifies the ZDD's Zigbee device type - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_DEVICE_TYPE
| zb_uint8_t zbd_zvd_comm_service_params_t::ext_pan_id[8] |
[00] Specifies the Zigbee network's extended PAN ID - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_TZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_EXT_PAN_ID
| zb_uint8_t zbd_zvd_comm_service_params_t::ieee_addr[8] |
[08] The 64-bit IEEE address of the ZDD - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_IEEE_ADDR
| zb_uint8_t zbd_zvd_comm_service_params_t::joining_method |
[07] Specifies the method the ZDD is instructed to use to join the network - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_JOINING_METHOD
| zb_uint8_t zbd_zvd_comm_service_params_t::link_key[16] |
[04] Specifies the Zigbee Link Key - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_LINK_KEY
| zb_uint8_t zbd_zvd_comm_service_params_t::link_key_flags_mask |
[18] Link Key flags zbd_aps_link_key_flags_mask_t
| zb_uint8_t zbd_zvd_comm_service_params_t::manage_joiners_cmd |
[15] Manage Joiners Command, as described in section 7.7.2.4.7 - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_MANAGE_JOINERS_CMD , see zbd_manage_joiners_cmd_e
| zb_uint8_t zbd_zvd_comm_service_params_t::manage_joiners_ieee[8] |
[16] The 64-bit IEEE address of the joiner ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_MANAGE_JOINERS_IEEE , see zbd_manage_joiners_cmd_e
| zb_uint8_t zbd_zvd_comm_service_params_t::manage_joiners_lnk_key[16] |
[17] Specifies the Zigbee Link Key associated with the joiner ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_MANAGE_JOINERS_LNK_KEY , see zbd_manage_joiners_cmd_e
| zb_uint8_t zbd_zvd_comm_service_params_t::nwk_active_key_seq_num |
[12] Current value of the nwkActiveKeySeqNumber attribute of the Zigbee NIB - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_ACTIVE_KEY_SEQ_NUM
| zb_uint16_t zbd_zvd_comm_service_params_t::nwk_addr |
[06] Specifies the ZDD's 16-bit Zigbee network address - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_ADDR
| zbd_nwk_channel_list_t zbd_zvd_comm_service_params_t::nwk_channel_list |
[02] Network Channel List - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_CHANNEL
| zb_uint8_t zbd_zvd_comm_service_params_t::nwk_key[16] |
[03] Specifies the Zigbee Network Key - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_KEY
| zbd_network_status_t zbd_zvd_comm_service_params_t::nwk_status_map |
[10] Contains a bitmap that indicates the ZDD's network status - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_STATUS_MAP
| zb_uint8_t zbd_zvd_comm_service_params_t::nwk_update_id |
[11] Current value of the nwkUpdateId attribute of the Zigbee NIB - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_NWK_UPDATE_ID
| zb_uint32_t zbd_zvd_comm_service_params_t::param_mask |
Parameter mask (used bits 0 to 16) - indicates what parameters of the request should be considered - zbd_zvd_comm_service_param_bitmasks_t.
| zb_uint16_t zbd_zvd_comm_service_params_t::short_pan_id |
[01] Specifies the Zigbee network's short PAN ID - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_SHORT_PAN_ID
| zbd_status_code_t zbd_zvd_comm_service_params_t::status_code |
[14] Status codes as described in section 7.7.2.4.6 - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_STATUS_CODE , zbd_status_code_s
| zb_uint8_t zbd_zvd_comm_service_params_t::tc_addr[8] |
[09] The 64-bit IEEE address of the Trust Center - ZBD_ZVD_COMM_SERVICE_PARAM_BITMASKS_T::ZBD_ZVD_COMM_SERVICE_PARAM_TC_ADDR