Logo
Developing with ZBOSS for Zigbee
zb_zgps_mapping_entry_additional_info_option_record_s Struct Reference

Mapping table entry additional info option record structure A.3.6.2.2 GPD application functionality translation Figure 83 – Format of the Option record field of the Translation Table entry. More...

#include <zboss_api_zgp.h>

Data Fields

zb_zgps_mapping_entry_additional_info_option_selector_t selector
 

Detailed Description

Mapping table entry additional info option record structure A.3.6.2.2 GPD application functionality translation Figure 83 – Format of the Option record field of the Translation Table entry.

Field Documentation

§ selector

zb_zgps_mapping_entry_additional_info_option_selector_t zb_zgps_mapping_entry_additional_info_option_record_s::selector

The documentation for this struct was generated from the following file: