Logo
Developing with ZBOSS for Zigbee

ZGP approve commissioning parameters. More...

#include <zboss_api_zdo.h>

Data Fields

zgp_approve_comm_params_tparams
 

Detailed Description

ZGP approve commissioning parameters.

Stack passes this parameter to application to notify about attempt GPD commissioning. Due to limited buffer memory, a pointer to the structure is passed.

Field Documentation

§ params

zgp_approve_comm_params_t* zb_zgp_signal_approve_comm_params_s::params

The documentation for this struct was generated from the following file: