Logo
Developing with ZBOSS for Zigbee
zb_zdo_signal_macsplit_dev_boot_params_s Struct Reference

MAC-Split device boot parameters. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint32_t dev_version
 
zb_ieee_addr_t extended_address
 

Detailed Description

MAC-Split device boot parameters.

MAC-Split passes this parameter to application when device is booted.

Field Documentation

§ dev_version

zb_uint32_t zb_zdo_signal_macsplit_dev_boot_params_s::dev_version

MAC-Split device version

§ extended_address

zb_ieee_addr_t zb_zdo_signal_macsplit_dev_boot_params_s::extended_address

The 64-bit (IEEE) address assigned to the device.


The documentation for this struct was generated from the following file: