Logo
Developing with ZBOSS for Zigbee
zb_zdo_signal_device_ready_for_interview_params_s Struct Reference

Device Ready For Interview signal parameters. More...

#include <zboss_api_zdo.h>

Data Fields

zb_ieee_addr_t long_addr
 
zb_uint16_t short_addr
 

Detailed Description

Device Ready For Interview signal parameters.

Field Documentation

§ long_addr

zb_ieee_addr_t zb_zdo_signal_device_ready_for_interview_params_s::long_addr

< Long Address of the device Short Address of the device

§ short_addr

zb_uint16_t zb_zdo_signal_device_ready_for_interview_params_s::short_addr

The documentation for this struct was generated from the following file: