Device Authorized signal parameters. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_ieee_addr_t | long_addr |
| zb_uint16_t | short_addr |
| zb_uint8_t | authorization_type |
| zb_uint8_t | authorization_status |
Device Authorized signal parameters.
| zb_uint8_t zb_zdo_signal_device_authorized_params_s::authorization_status |
| zb_uint8_t zb_zdo_signal_device_authorized_params_s::authorization_type |
Status of the authorization procedure (depends on zdo_authorization_type)
| zb_ieee_addr_t zb_zdo_signal_device_authorized_params_s::long_addr |
< Long Address of the updated device Short Address of the updated device
| zb_uint16_t zb_zdo_signal_device_authorized_params_s::short_addr |
Type of the authorization procedure, zdo_authorization_type