Logo
Developing with ZBOSS for Zigbee
zb_zdo_next_panid_change_parameters_s Struct Reference

Next PAN ID change parameters Stack sends set_configuration_req to the device with set values. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint16_t dst_addr
 
zb_uint16_t next_panid_change
 

Detailed Description

Next PAN ID change parameters Stack sends set_configuration_req to the device with set values.

Field Documentation

§ dst_addr

zb_uint16_t zb_zdo_next_panid_change_parameters_s::dst_addr

destination address

§ next_panid_change

zb_uint16_t zb_zdo_next_panid_change_parameters_s::next_panid_change

nwkNextPanId, this field indicates the next PAN ID that will be used once a Network Update command is received to change PAN IDs. A value 0xFFFF allows any PAN ID to be accepted


The documentation for this struct was generated from the following file: