Logo
Developing with ZBOSS for Zigbee
zb_zdo_clear_all_bind_req_param_s Struct Reference

Parameters for zdo_clear_all_bind_req. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint16_t dst_addr
 
zb_uint8_t eui64_count
 
zb_ieee_addr_t eui64_list [(5u)]
 

Detailed Description

Parameters for zdo_clear_all_bind_req.

Field Documentation

§ dst_addr

zb_uint16_t zb_zdo_clear_all_bind_req_param_s::dst_addr

destination address

§ eui64_count

zb_uint8_t zb_zdo_clear_all_bind_req_param_s::eui64_count

eui64 count

§ eui64_list

zb_ieee_addr_t zb_zdo_clear_all_bind_req_param_s::eui64_list[(5u)]

eui64 list, a value 0xFFFFFFFFFFFFFFFF is a wildcard


The documentation for this struct was generated from the following file: