Logo
Developing with ZBOSS for Zigbee
zb_zdo_beacon_survey_potential_parents_t Struct Reference

R23, I.3.5 Potential Parents TLV. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint16_t current_parent
 
zb_uint8_t current_parent_lqa
 
zb_uint8_t count_potential_parents
 
zb_zcl_wwah_beacon_survey_t parent_list [5U]
 

Detailed Description

R23, I.3.5 Potential Parents TLV.

This TLV is 3 to 13 bytes in length and indicates the number of available parents in radio range. A maximum number of 5 parents is supported for this TLV. The list of potential parents SHALL be ordered as described in 3.6.1.3.2.

Field Documentation

§ count_potential_parents

zb_uint8_t zb_zdo_beacon_survey_potential_parents_t::count_potential_parents

Potential parents list

§ current_parent

zb_uint16_t zb_zdo_beacon_survey_potential_parents_t::current_parent

< r23 Short address of the parent. Filled by r23 Beacon Survey only

§ current_parent_lqa

zb_uint8_t zb_zdo_beacon_survey_potential_parents_t::current_parent_lqa

r23 - LQA of the current parent. Filled by r23 Beacon Survey only Count of potential parents. Valid range [0..5] for r23-only build, [0..10] for WWAH (Indeed, WWAH requires to put there as much info as can be put into the single frame)

§ parent_list

zb_zcl_wwah_beacon_survey_t zb_zdo_beacon_survey_potential_parents_t::parent_list[5U]

The documentation for this struct was generated from the following file: