Developing with ZBOSS for Zigbee
Data Fields
zb_zdo_app_signal_hdr_s Struct Reference
Zigbee stack API
»
Application structure & commissioning start
»
ZBOSS commissioning signals handler
#include <zboss_api_zdo.h>
Data Fields
zb_uint32_t
sig_type
Detailed Description
Application signal header
Field Documentation
§
sig_type
zb_uint32_t
zb_zdo_app_signal_hdr_s::sig_type
The documentation for this struct was generated from the following file:
/conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/
zboss_api_zdo.h
Copyright (c) 2012-2022 DSR Corporation, Golden CO, USA.
http://www.dsr-zboss.com
http://www.dsr-corporation.com
ZBOSS documentation. Wed Oct 29 2025.