Logo
Developing with ZBOSS for Zigbee
zb_zdo_active_scan_resp_s Struct Reference

Parameters for active_scan_resp. More...

#include <zboss_api_zdo.h>

Data Fields

zb_ret_t status
 
zb_uint8_t network_count
 

Detailed Description

Parameters for active_scan_resp.

Field Documentation

§ network_count

zb_uint8_t zb_zdo_active_scan_resp_s::network_count

Number of discovered networks

§ status

zb_ret_t zb_zdo_active_scan_resp_s::status

Our error or MAC status codes (see Table 3-11 NLME-NETWORK-DISCOVERY.confirm Parameters: Any status value returned with the MLME-SCAN.confirm primitive.)


The documentation for this struct was generated from the following file: