Logo
Developing with ZBOSS for Zigbee
zb_zcl_wwah_beacon_survey_s Struct Reference

#include <zboss_api_zdo.h>

Data Fields

zb_uint16_t device_short
 
zb_int8_t rssi
 
zb_uint8_t lqi
 
zb_uint8_t classification_mask
 

Detailed Description

Beacon survey result for a single potential parent. Common deniminator for r23 and WWAH.

Field Documentation

§ classification_mask

zb_uint8_t zb_zcl_wwah_beacon_survey_s::classification_mask

§ device_short

zb_uint16_t zb_zcl_wwah_beacon_survey_s::device_short

§ lqi

zb_uint8_t zb_zcl_wwah_beacon_survey_s::lqi

§ rssi

zb_int8_t zb_zcl_wwah_beacon_survey_s::rssi

RSSI of the beacon, expressed in dBm. Filled by WWAH only


The documentation for this struct was generated from the following file: