TransferData payload. This structure presents custom implementation of Transfer Data command payload defined in SE spec. More...
#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_zcl_tunneling_transfer_data_hdr_t | hdr |
| zb_uint8_t | data_size |
| zb_uint8_t * | tun_data |
| Octet containing the data to be transferred through the tunnel in the format of the communication protocol for which the tunnel has been requested and opened. The payload contains the assembled data exactly as it was sent by the client. Theoretically, its length is solely limited through the fragmentation algorithm and the RX/TX transfer buffer sizes within the communication partners. The content of the payload is up to the application sending the data. It is neither guaranteed, that it contains a complete PDU nor is any other assumption on its internal format made. This is left up to the implementer of the specific protocol tunnel behavior. More... | |
TransferData payload. This structure presents custom implementation of Transfer Data command payload defined in SE spec.
| zb_uint8_t zb_zcl_tunneling_transfer_data_payload_s::data_size |
Size of tun_data
| zb_zcl_tunneling_transfer_data_hdr_t zb_zcl_tunneling_transfer_data_payload_s::hdr |
| zb_uint8_t* zb_zcl_tunneling_transfer_data_payload_s::tun_data |
Octet containing the data to be transferred through the tunnel in the format of the communication protocol for which the tunnel has been requested and opened. The payload contains the assembled data exactly as it was sent by the client. Theoretically, its length is solely limited through the fragmentation algorithm and the RX/TX transfer buffer sizes within the communication partners. The content of the payload is up to the application sending the data. It is neither guaranteed, that it contains a complete PDU nor is any other assumption on its internal format made. This is left up to the implementer of the specific protocol tunnel behavior.