Logo
Developing with ZBOSS for Zigbee
zb_zcl_tunneling_request_tunnel_s Struct Reference

RequestTunnel command payload More...

#include <zb_zcl_tunneling.h>

Data Fields

zb_uint8_t protocol_id
 An enumeration representing the identifier of the metering communication protocol for which the tunnel is requested. More...
 
zb_uint16_t manufacturer_code
 A code that is allocated by the Zigbee Alliance, relating the manufacturer to a device and – for the tunneling - a manufacturer specific protocol. The parameter is ignored when the ProtocolID value is less than 200. This allows for 55 manufacturer-defined protocols for each manufacturer to be defined. A value of 0xFFFF indicates that the Manufacturer Code is not used. More...
 
zb_bool_t flow_control_support
 A boolean type parameter that indicates whether flow control support is requested from the tunnel (ZB_TRUE) or not (ZB_FALSE). The default value is FALSE (no flow control). More...
 
zb_uint16_t max_incoming_transfer_size
 A value that defines the size, in octets, of the maximum data packet that can be transferred to the client in the payload of a single TransferData command. More...
 

Detailed Description

RequestTunnel command payload

See also
SE spec, subclause D.6.2.4.1.2

Field Documentation

§ flow_control_support

zb_bool_t zb_zcl_tunneling_request_tunnel_s::flow_control_support

A boolean type parameter that indicates whether flow control support is requested from the tunnel (ZB_TRUE) or not (ZB_FALSE). The default value is FALSE (no flow control).

§ manufacturer_code

zb_uint16_t zb_zcl_tunneling_request_tunnel_s::manufacturer_code

A code that is allocated by the Zigbee Alliance, relating the manufacturer to a device and – for the tunneling - a manufacturer specific protocol. The parameter is ignored when the ProtocolID value is less than 200. This allows for 55 manufacturer-defined protocols for each manufacturer to be defined. A value of 0xFFFF indicates that the Manufacturer Code is not used.

§ max_incoming_transfer_size

zb_uint16_t zb_zcl_tunneling_request_tunnel_s::max_incoming_transfer_size

A value that defines the size, in octets, of the maximum data packet that can be transferred to the client in the payload of a single TransferData command.

§ protocol_id

zb_uint8_t zb_zcl_tunneling_request_tunnel_s::protocol_id

An enumeration representing the identifier of the metering communication protocol for which the tunnel is requested.

See also
zb_zcl_tunneling_protocol_id_e

The documentation for this struct was generated from the following file: